psa_drv_se_key_derivation_t Struct Reference
A struct containing all of the function pointers needed to for secure element key derivation and agreement.
PSA Crypto API implementations should populate instances of the table as appropriate upon startup.
If one of the functions is not implemented, it should be set to NULL.
Definition at line 1263
of file crypto_se_driver.h
.
#include <
crypto_se_driver.h
>
Field Documentation
size_t psa_drv_se_key_derivation_t::context_size |
The driver-specific size of the key derivation context
Definition at line 1265
of file crypto_se_driver.h
.
psa_drv_se_key_derivation_collateral_t psa_drv_se_key_derivation_t::p_collateral |
Function that sets key derivation collateral
Definition at line 1269
of file crypto_se_driver.h
.
psa_drv_se_key_derivation_derive_t psa_drv_se_key_derivation_t::p_derive |
Function that performs a final key derivation step
Definition at line 1271
of file crypto_se_driver.h
.
psa_drv_se_key_derivation_export_t psa_drv_se_key_derivation_t::p_export |
Function that perforsm a final key derivation or agreement and exports the key
Definition at line 1274
of file crypto_se_driver.h
.
psa_drv_se_key_derivation_setup_t psa_drv_se_key_derivation_t::p_setup |
Function that performs a key derivation setup
Definition at line 1267
of file crypto_se_driver.h
.
The documentation for this struct was generated from the following file:
crypto_se_driver.h