psa_drv_se_key_management_t Struct Reference
A struct containing all of the function pointers needed to for secure element key management.
PSA Crypto API implementations should populate instances of the table as appropriate upon startup or at build time.
If one of the functions is not implemented, it should be set to NULL.
Definition at line 1120
of file crypto_se_driver.h
.
#include <
crypto_se_driver.h
>
Field Documentation
psa_drv_se_allocate_key_t psa_drv_se_key_management_t::p_allocate |
Function that allocates a slot for a key.
Definition at line 1122
of file crypto_se_driver.h
.
psa_drv_se_destroy_key_t psa_drv_se_key_management_t::p_destroy |
Function that performs a key destroy operation
Definition at line 1130
of file crypto_se_driver.h
.
psa_drv_se_export_key_t psa_drv_se_key_management_t::p_export |
Function that performs a key export operation
Definition at line 1132
of file crypto_se_driver.h
.
psa_drv_se_export_key_t psa_drv_se_key_management_t::p_export_public |
Function that performs a public key export operation
Definition at line 1134
of file crypto_se_driver.h
.
psa_drv_se_generate_key_t psa_drv_se_key_management_t::p_generate |
Function that performs a generation
Definition at line 1128
of file crypto_se_driver.h
.
psa_drv_se_import_key_t psa_drv_se_key_management_t::p_import |
Function that performs a key import operation
Definition at line 1126
of file crypto_se_driver.h
.
psa_drv_se_validate_slot_number_t psa_drv_se_key_management_t::p_validate_slot_number |
Function that checks the validity of a slot for a key.
Definition at line 1124
of file crypto_se_driver.h
.
The documentation for this struct was generated from the following file:
crypto_se_driver.h