mbedtls_ccm_context Struct ReferenceCryptography Hardware Acceleration Plugins > Accelerated AES-CCM AEAD Cipher

The CCM context-type definition. The CCM context is passed to the APIs called.

Definition at line 43 of file ccm_alt.h.

#include <ccm_alt.h>

Data Fields

uint8_t key [32]
 
uint32_t keybits
 

Field Documentation

uint8_t mbedtls_ccm_context::key[32]

The key in use.

Definition at line 44 of file ccm_alt.h.

uint32_t mbedtls_ccm_context::keybits

Definition at line 45 of file ccm_alt.h.


The documentation for this struct was generated from the following file:
  • ccm_alt.h