mbedtls_trng_context Struct ReferenceRandom number generator (RNG) module > True Random Number Generator (TRNG) Plugin

TRNG context structure.

Definition at line 150 of file trng.h.

#include <trng.h>

Data Fields

TRNG_TypeDef * trng
 
void(* test_error_callback )(void *user_arg, int error_code)
 
void * test_error_callback_user_arg
 

Field Documentation

void(* mbedtls_trng_context::test_error_callback) (void *user_arg, int error_code)

User defined callback to be called when an internal TRNG test fails.

Definition at line 156 of file trng.h.

void* mbedtls_trng_context::test_error_callback_user_arg

User defined argument to TRNG test error callback.

Definition at line 159 of file trng.h.

TRNG_TypeDef* mbedtls_trng_context::trng

TRNG register block pointer.

Definition at line 153 of file trng.h.


The documentation for this struct was generated from the following file:
  • trng.h