EblBootloader_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format

Description

GBL bootloader tag type.

Definition at line 57 of file btl_gbl_format.h.

#include <btl_gbl_format.h>

Data Fields

EblTagHeader_t header
 Tag ID and length.
 
uint32_t bootloaderVersion
 Version number of the bootloader.
 
uint32_t address
 Address of the bootloader.
 
uint8_t * data
 Array of data for bootloader upgrade.
 

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h