EblEncryptionData_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format

Description

GBL encryption data tag type.

Definition at line 108 of file btl_gbl_format.h.

#include <btl_gbl_format.h>

Data Fields

EblTagHeader_t header
 Tag ID and length.
 
uint8_t * encryptedEblData
 Encrypted data.
 

Field Documentation

uint8_t* EblEncryptionData_t::encryptedEblData

Encrypted data.

After decryption, this data must represent one or more complete unencrypted GBL tags.

Definition at line 110 of file btl_gbl_format.h.


The documentation for this struct was generated from the following file:
  • btl_gbl_format.h