EblEncryptionHeader_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format

Description

GBL encryption header tag type.

Definition at line 92 of file btl_gbl_format.h.

#include <btl_gbl_format.h>

Data Fields

EblTagHeader_t header
 Tag ID and length.
 
uint32_t version
 Version of the GBL spec used in this file.
 
uint32_t magicWord
 Magic word (GBL_IMAGE_MAGIC_WORD)
 
uint32_t encryptionType
 Type of encryption used. 1 = AES-CTR.
 

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h