EblEncryptionInitAesCcm_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format

Description

GBL encryption init tag type. Used with AES-CCM encryption.

Definition at line 100 of file btl_gbl_format.h.

#include <btl_gbl_format.h>

Data Fields

EblTagHeader_t header
 Tag ID and length.
 
uint32_t msgLen
 Length of the cipher text in bytes.
 
uint8_t nonce [12]
 Random nonce used for AES-CTR in this message.
 

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h