EblTagHeader_t Struct ReferenceComponents > Image Parser > GBL Parser > GBL Format

Description

GBL tag header. Must be the first element in all GBL tags.

Definition at line 38 of file btl_gbl_format.h.

#include <btl_gbl_format.h>

Data Fields

uint32_t tagId
 Tag ID.
 
uint32_t length
 Length (in bytes) of the rest of the tag.
 

The documentation for this struct was generated from the following file:
  • btl_gbl_format.h