Developing and Debugging a Gecko Bootloader#
These pages provide detailed information for Gecko Bootloader Developers.
Silicon Labs Gecko Bootloader User's Guide for GSDK 4.0 and Higher (PDF): Describes the high-level implementation of the Silicon Labs Gecko Bootloader for EFM32 and EFR32 Series 1 and Series 2 microcontrollers, SoCs (System on Chips) and NCPs (Network Co-Processors), and provides information on different aspects of configuring the Gecko Bootloader.
Transitioning to the Updated Gecko Bootloader in GSDK 4.0 and Higher (PDF): Gecko Bootloader v2.x, introduced in GSDK 4.0, contains a number of changes compared to Gecko Bootloader v1.x. This describes the differences between the versions, including how to configure the new Gecko Bootloader in Simplicity Studio 5.
Simplicity Commander Reference Guide (PDF): Describes how and when to use the Command-Line Interface (CLI) of Simplicity Commander. Simplicity Commander supports all EFR32 Wireless SoCs, EFR32 Wireless SoC modules (such as the MGM111 or MGM12P), EFM32 MCU families, and EM3xx Wireless SOCs.