Protocol-Specific Information#
These pages provide information about using a Gecko Bootloader in the context of a specific protocol. Additional protocol-specific content is available through the docs.silabs.com homepage.
Silicon Labs Bluetooth: Includes detailed information on using the Gecko Bootloader with Silicon Labs Bluetooth applications.
Silicon Labs Connect: Provides information on using the Silicon Labs Gecko Bootloader with Connect.
Zigbee EmberZNet: Includes detailed information on using the Silicon Labs Gecko Bootloader with EmberZNet.