Protocol-Specific Information#

These pages provide information about using a Gecko Bootloader in the context of a specific protocol. Additional protocol-specific content is available through the docs.silabs.com homepage.

  • Silicon Labs Bluetooth: Includes detailed information on using the Gecko Bootloader with Silicon Labs Bluetooth applications.

  • Silicon Labs Connect: Provides information on using the Silicon Labs Gecko Bootloader with Connect.

  • Zigbee EmberZNet: Includes detailed information on using the Silicon Labs Gecko Bootloader with EmberZNet.