Silicon Labs
mcu/5.4/efm32hg/structBlock-TypeDef
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
Results 1-5 of 5 for mcu/5.4/efm32hg/structBlock-TypeDef in 0.05 seconds
Advertiser | Bluetooth Stack API Reference | Bluetooth LE | v8.0.0 | Silicon Labs
https://docs.silabs.com/.../sl-bt-adverti...
// Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... of file /mnt/raid/workspaces/ws.RGfN6W7IO/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
sl_bt_evt_scanner_scan_reportScanner | Scanner | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/.../a00...
// Bluetooth LE//Version 5.0 //API Reference //Commands & Events ... Bits 3.4 : Reserved for future Bits 5.6 : data completeness* 00: Complete ... Value 0 indicates no periodic advertising.
Adaptive Frequency Hopping | System & Performance | Bluetooth LE | v5.0 | Silicon Labs
https://docs.silabs.com/.../adaptive-frequency-hopp...
Bluetooth functions in the 2.4 GHz frequency range. ... Channel map update procedure is part of the Bluetooth 4.0 specification. ... Bluetooth Low Energy has two channel selection algorithms.
TX Power Limitations for Regulatory Compliance (ETSI, FCC) | System & Performance | Bluetooth LE | v3.1 | Silicon Labs
https://docs.silabs.com/.../tx-power-limitations-for-regulatory-compliance-etsi-...
// Bluetooth LE//Version 3.1 //General ... Because Bluetooth stack follows strict regulations, the maximum output power is 10 dBm in those cases when AFH is not enabled (or AFH is enabled but ...
Bluetooth Advertising Data Basics - Silicon Labs
https://www.silabs.com/.../bluetooth-advertising-data-bas...
This Bluetooth advertising training reviews the basics of this fundamental Bluetooth LE operation, and introduces customizing your advertising ... Bluetooth 102 - Advertising Training Series
ProductWireless Resource TypeWritten Materials
    Results 1-5 of 5 for mcu/5.4/efm32hg/structBlock-TypeDef