USB_CompatFunctionDesc_t Struct Reference
Compatible ID Function Descriptor Typedef.
Definition at line 160
of file em_usbxpress_descriptors.h
.
#include <
em_usbxpress_descriptors.h
>
Data Fields | |
char | compatibleID [8] |
String describing the compatible ID. | |
uint8_t | firstInterfaceNumber |
uint8_t | reserved1 |
Reserved (unused) | |
uint8_t | reserved2 [6] |
Reserved (unused) | |
char | subCompatibleID [8] |
String describing the sub compatible ID. | |
Field Documentation
uint8_t USB_CompatFunctionDesc_t::firstInterfaceNumber |
Interface number for extended compatibility feature descriptor
Definition at line 161
of file em_usbxpress_descriptors.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/middleware/usbxpress/inc/
em_usbxpress_descriptors.h