USB_ExtendedCompatIdOsFeatureDesc_t Struct Reference

Compatible ID Feature Descriptor Typedef.

Definition at line 172 of file em_usbxpress_descriptors.h.

#include <em_usbxpress_descriptors.h>

Data Fields

uint16_t bcdVersion
 1.00 -> 0x0100
 
uint8_t count
 Number of functions sections.
 
const USB_CompatFunctionDesc_t ecid [NUM_IFCS_WITH_EXT_COMPAT]
 Extended capabilities.
 
uint16_t index
 
uint32_t length
 Size of this struct = 16 + bCount*24.
 
uint8_t reserved1 [7]
 Reserved (unused)
 

Field Documentation

uint16_t USB_ExtendedCompatIdOsFeatureDesc_t::index

Command index - 0x04 for extended compatibility ID

Definition at line 175 of file em_usbxpress_descriptors.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/middleware/usbxpress/inc/em_usbxpress_descriptors.h