Silicon Labs
mcu/5.4/structACMP-VBConfig-TypeDef
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
Results 1-5 of 5 for mcu/5.4/structACMP-VBConfig-TypeDef in 0.18 seconds
Bluetooth SDK Release Notes
https://www.silabs.com/.../bt-software-release-notes-7.3.0.0....
SDK or on the TECH DOCS tab on https://www.silabs.com/developers/bluetooth-low-energy ... All RCP apps now by default support 192 µsec turnaround time for non-enhanced acks while still using ...
Resource TypeRelease Notes
Gecko OS Commands Silicon Labs
https://docs.silabs.com/.../comma...
0 - the request failed, the contains the error message ... c rc: CRC32 checksum of the file data, in hex format 2 . ... Gecko OS lists all the variables in that group with their values.
Gecko OS 4.2 Command API Silicon Labs
https://docs.silabs.com/.../...
Gecko OS 4.2 Command API The Command API documentation provides details of commands ... Variables Examples See Gecko OS General Overview for a description of the general structure and features ...
Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../update-and-recov...
The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated via the ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults counter
ProductWireless Resource TypeSoftware API documentation
BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
https://docs.silabs.com/.../comma...
Example Example usage. Alphabetical List of Commands ... All cleared and new devices will need to complete a pairing procedure on their next ... os pins can only use the strong drive strength.
ProductWireless Resource TypeSoftware API documentation
    Results 1-5 of 5 for mcu/5.4/structACMP-VBConfig-TypeDef