USB_ExtendedCompatIdOsFeatureDesc_t Struct Reference
Compatible ID Feature Descriptor Typedef.
Definition at line 172
of file em_usbxpress_descriptors.h
.
#include <
em_usbxpress_descriptors.h
>
Data Fields | |
uint16_t | bcdVersion |
1.00 -> 0x0100 | |
uint8_t | count |
Number of functions sections. | |
const USB_CompatFunctionDesc_t | ecid [NUM_IFCS_WITH_EXT_COMPAT] |
Extended capabilities. | |
uint16_t | index |
uint32_t | length |
Size of this struct = 16 + bCount*24. | |
uint8_t | reserved1 [7] |
Reserved (unused) | |
Field Documentation
uint16_t USB_ExtendedCompatIdOsFeatureDesc_t::index |
Command index - 0x04 for extended compatibility ID
Definition at line 175
of file em_usbxpress_descriptors.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/middleware/usbxpress/inc/
em_usbxpress_descriptors.h