Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
ProductWirelessResource TypeSoftware API documentation
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... network.tls.ca_cert spi.master.active_gpio spi.master.active_level system.cmd.buffered
ProductWirelessResource TypeSoftware API documentation
... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. May be one of the following types: drvst : Strong drive ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS Commands This page lists the Gecko OS Command API with a full description of how to use each ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Results 1-5 of 5 for mcu/5.5/structLESENSE-CH-TypeDef