Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Examples: network/ethernet_bridge/main.c . ◆ gos_cmd_issue_with_data()
ProductWirelessResource TypeSoftware API documentation
network_down network_lookup network_flush network_restart ... TCP tcp_client tcp_server tls_client ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Gecko OS is part of a larger sophisticated application framework installed on all ... tcp.client.connect_timeout tcp.client.local_port tcp.client.retries tcp.client.retry_period uart.baud
ProductWirelessResource TypeSoftware API documentation
os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren ) ... Returns the RSSI value from the latest received packet of the current active ...
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for mcu/5.5/structMSC-ExecConfig-TypeDef