... and RTS locations by setting portLocationCts and portLocationRts in the init struct. ... data, UARTDRV_Count_t maxCount ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollersResource TypeSoftware API documentation
// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
You should avoid using it in production. ... Functions sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables sl_iostream_t * sl_iostream_rtt_handle ... ) RTT Stream init. Returns
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... is the recommended device independent crypto API and should be used whenever possible ... sl_se_otp_init_t otp_settings_init = SL_SE_OTP_INIT_DEFAULT;