Silicon Labs
mcu/5.6/group-RTCDRV
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
Results 1-5 of 5 for mcu/5.6/group-RTCDRV in 0.16 seconds
Sleep Timer | API Documentation | Gecko Platform | v4.4.1 | Silicon Labs
https://docs.silabs.com/.../sleepti...
// Gecko Platform//Version 4.4.1 //Services ... A 64-bits tick counter is accessible through the ... All API functions can be called from within interrupt handlers. ... Description N/A handle
UARTDRV - UART Driver - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-uart...
A template for this file, containing default values, is in the emdrv/config folder. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollers Resource TypeSoftware API documentation
Project Configurator and Gecko Platform
https://www.silabs.com/.../project-configuration-gecko-platform-training....
... -platform/latest/driver/api/group-uartdrv https://docs.silabs.com/gecko-platform/latest/driver/api/group-ustimer Gecko Platform – Service ... Platform Services Detail Device Initialization
I/O Stream RTT - v4.2 - Gecko Platform API Documentation Silicon Labs
https://docs.silabs.com/.../group-iostream-...
RTT module uses a control block structure located in RAM memory with a specific ID so that it can be discovered when a ... sl_status_t sl_iostream_rtt_init (void) RTT Stream init. Variables
ProductMicrocontrollers Resource TypeSoftware API documentation
SE Manager | API Documentation | Platform | v5.0.1 | Silicon Labs
https://docs.silabs.com/.../sl-se-mana...
// Platform//Version 5.0.1 //Security ... PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... A counter in the tamper filter is increased.
    Results 1-5 of 5 for mcu/5.6/group-RTCDRV