// Bluetooth LE//Version 6.1.0 //Bluetooth API Reference Guide //System ... sl_bt_cmd_system_set_identity_address_id 0x13010020 ... Bluetooth identity address in little endian format
// Bluetooth LE//Version 6.0.0 //Bluetooth API Reference Guide //System ... sl_bt_cmd_system_set_identity_address_id 0x13010020 ... Bluetooth identity address in little endian format
Set the maximum size of ATT Message Transfer Units (MTU). ... is a reliable write (by Bluetooth Core Specification Volume 3, Part G, 4.9.5). Parameters [in]| `connection`| Connection handle
8.1.0 Connection# Connection. ... sl_bt_cmd_connection_set_parameters_id 0x06060020 ... Set the supervision timeout at a value which allows communication attempts over at least a few ...
// Bluetooth LE//Version 8.0.0 //Bluetooth Stack API Reference //Advertiser ... sl_bt_cmd_advertiser_clear_random_address_id 0x11040020 ... Time range: 10 ms to 655.35 s Default : 0 uint8_t