sl_bt_cmd_system_linklayer_configure_id 0x0e010020 ... Bluetooth identity address in little endian format ... Read the Bluetooth identity address used by the device, which can be a public or ...
8.1.0 Connection# Connection. ... sl_bt_cmd_connection_read_channel_map_id 0x07060020 ... [in] connection Connection Handle Read link layer features supported by the remote device.
// Bluetooth LE//Version 6.0.0 //Bluetooth API Reference Guide //System ... sl_bt_cmd_system_linklayer_configure_id 0x0e010020 ... Bluetooth identity address in little endian format
sl_status_t | sl_bt_gatt_server_send_user_read_response (uint8_t connection, uint16_t characteristic, uint8_t att_errorcode, size_ ... Read the type of an attribute from a local GATT database.
Training ... Support ... Register ... sl_bt_cmd_advertiser_set_channel_map_id 0x04040020 ... [in] channel_map Advertising channel map which determines, which of the three channels will be used ...
Results 1-5 of 5 for mcu/5.7/structCORE-nvicMask-t