CAN_MIR_TypeDef Struct ReferenceDevicesDevices > | CAN

CAN_MIR CAN MIR Register

.

Definition at line 46 of file efm32gg11b_can_mir.h.

#include <efm32gg11b_can_mir.h>

Data Fields

__IOM uint32_t ARB
 
__IOM uint32_t CMDMASK
 
__IOM uint32_t CMDREQ
 
__IOM uint32_t CTRL
 
__IOM uint32_t DATAH
 
__IOM uint32_t DATAL
 
__IOM uint32_t MASK
 
uint32_t RESERVED0 [1U]
 

Field Documentation

__IOM uint32_t CAN_MIR_TypeDef::ARB

Interface Arbitration Register

Definition at line 49 of file efm32gg11b_can_mir.h.

Referenced by CAN_ConfigureMessageObject(), CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), CAN_SendMessage(), and CAN_SetIdAndFilter().

__IOM uint32_t CAN_MIR_TypeDef::CMDMASK

Interface Command Mask Register

Definition at line 47 of file efm32gg11b_can_mir.h.

Referenced by CAN_AbortSendMessage(), CAN_ConfigureMessageObject(), CAN_MessageLost(), CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), CAN_SendMessage(), and CAN_SetIdAndFilter().

__IOM uint32_t CAN_MIR_TypeDef::CMDREQ

Interface Command Request Register

Definition at line 53 of file efm32gg11b_can_mir.h.

Referenced by CAN_ReadyWait(), CAN_Reset(), and CAN_SendRequest().

__IOM uint32_t CAN_MIR_TypeDef::CTRL

Interface Message Control Register

Definition at line 50 of file efm32gg11b_can_mir.h.

Referenced by CAN_AbortSendMessage(), CAN_ConfigureMessageObject(), CAN_MessageLost(), CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), CAN_SendMessage(), and CAN_SetIdAndFilter().

__IOM uint32_t CAN_MIR_TypeDef::DATAH

Interface Data B Register

Definition at line 52 of file efm32gg11b_can_mir.h.

Referenced by CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), and CAN_WriteData().

__IOM uint32_t CAN_MIR_TypeDef::DATAL

Interface Data a Register

Definition at line 51 of file efm32gg11b_can_mir.h.

Referenced by CAN_ReadMessage(), CAN_Reset(), CAN_ResetMessages(), and CAN_WriteData().

__IOM uint32_t CAN_MIR_TypeDef::MASK

Interface Mask Register

Definition at line 48 of file efm32gg11b_can_mir.h.

Referenced by CAN_Reset(), CAN_ResetMessages(), and CAN_SetIdAndFilter().

uint32_t CAN_MIR_TypeDef::RESERVED0[1U]

Reserved future

Definition at line 54 of file efm32gg11b_can_mir.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/efm32gg11b_can_mir.h