USB_ExtendedPropertiesDescriptor_t Struct Reference
Extended Properties Descriptor Typedef.
Definition at line 189
of file em_usbxpress_descriptors.h
.
#include <
em_usbxpress_descriptors.h
>
Data Fields | |
uint16_t | bcdVersion |
1.00 -> 0x0100 | |
uint16_t | count |
Number of properties. | |
uint16_t | index |
0x05 for extended property | |
uint8_t | propertyData2 [GUID_PROPERTY_LEN ] |
Property data. | |
uint32_t | propertyDataLength |
Length the property data. | |
uint32_t | propertyDataType |
Data type of this property. | |
uint8_t | propertyName [GUID_PROPERTY_NAME_LEN ] |
Name of this property. | |
uint16_t | propertyNameLength |
Length of the name of this property. | |
uint32_t | size2 |
Size of this property descriptor. | |
uint32_t | wLength |
Size of this struct. | |
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/middleware/usbxpress/inc/
em_usbxpress_descriptors.h