ACMP_TypeDef Struct ReferenceDevices > ACMP

ACMP Register Declaration.

Definition at line 46 of file efr32bg21_acmp.h.

#include <efr32bg21_acmp.h>

Data Fields

__IOM uint32_t CFG
 
__IOM uint32_t CFG_CLR
 
__IOM uint32_t CFG_SET
 
__IOM uint32_t CFG_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IOM uint32_t INPUTCTRL
 
__IOM uint32_t INPUTCTRL_CLR
 
__IOM uint32_t INPUTCTRL_SET
 
__IOM uint32_t INPUTCTRL_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
uint32_t RESERVED0 [1015U]
 
uint32_t RESERVED1 [1015U]
 
uint32_t RESERVED2 [1015U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IM uint32_t SYNCBUSY
 
__IM uint32_t SYNCBUSY_CLR
 
__IM uint32_t SYNCBUSY_SET
 
__IM uint32_t SYNCBUSY_TGL
 

Field Documentation

__IOM uint32_t ACMP_TypeDef::CFG

Configuration register

Definition at line 49 of file efr32bg21_acmp.h.

Referenced by ACMP_CapsenseInit(), ACMP_Init(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::CFG_CLR

Configuration register

Definition at line 69 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::CFG_SET

Configuration register

Definition at line 59 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::CFG_TGL

Configuration register

Definition at line 79 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::CTRL

Control Register

Definition at line 50 of file efr32bg21_acmp.h.

Referenced by ACMP_CapsenseInit(), ACMP_Disable(), ACMP_Enable(), ACMP_GPIOSetup(), ACMP_Init(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::CTRL_CLR

Control Register

Definition at line 70 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::CTRL_SET

Control Register

Definition at line 60 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::CTRL_TGL

Control Register

Definition at line 80 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::EN

ACMP enable

Definition at line 48 of file efr32bg21_acmp.h.

Referenced by ACMP_CapsenseChannelSet(), ACMP_ChannelSet(), and ACMP_Disable().

__IOM uint32_t ACMP_TypeDef::EN_CLR

ACMP enable

Definition at line 68 of file efr32bg21_acmp.h.

Referenced by ACMP_Disable().

__IOM uint32_t ACMP_TypeDef::EN_SET

ACMP enable

Definition at line 58 of file efr32bg21_acmp.h.

Referenced by ACMP_Enable().

__IOM uint32_t ACMP_TypeDef::EN_TGL

ACMP enable

Definition at line 78 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 54 of file efr32bg21_acmp.h.

Referenced by ACMP_IntDisable(), ACMP_IntEnable(), ACMP_IntGetEnabled(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 74 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 64 of file efr32bg21_acmp.h.

Referenced by ACMP_IntEnable().

__IOM uint32_t ACMP_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 84 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efr32bg21_acmp.h.

Referenced by ACMP_IntGet(), and ACMP_IntGetEnabled().

__IOM uint32_t ACMP_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 73 of file efr32bg21_acmp.h.

Referenced by ACMP_IntClear(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 63 of file efr32bg21_acmp.h.

Referenced by ACMP_IntSet().

__IOM uint32_t ACMP_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 83 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::INPUTCTRL

Input Control Register

Definition at line 51 of file efr32bg21_acmp.h.

Referenced by ACMP_CapsenseChannelSet(), ACMP_CapsenseInit(), ACMP_ChannelSet(), ACMP_Init(), and ACMP_Reset().

__IOM uint32_t ACMP_TypeDef::INPUTCTRL_CLR

Input Control Register

Definition at line 71 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::INPUTCTRL_SET

Input Control Register

Definition at line 61 of file efr32bg21_acmp.h.

__IOM uint32_t ACMP_TypeDef::INPUTCTRL_TGL

Input Control Register

Definition at line 81 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::IPVERSION

IP version ID

Definition at line 47 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::IPVERSION_CLR

IP version ID

Definition at line 67 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::IPVERSION_SET

IP version ID

Definition at line 57 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::IPVERSION_TGL

IP version ID

Definition at line 77 of file efr32bg21_acmp.h.

uint32_t ACMP_TypeDef::RESERVED0[1015U]

Reserved for future use

Definition at line 56 of file efr32bg21_acmp.h.

uint32_t ACMP_TypeDef::RESERVED1[1015U]

Reserved for future use

Definition at line 66 of file efr32bg21_acmp.h.

uint32_t ACMP_TypeDef::RESERVED2[1015U]

Reserved for future use

Definition at line 76 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::STATUS

Status Register

Definition at line 52 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::STATUS_CLR

Status Register

Definition at line 72 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::STATUS_SET

Status Register

Definition at line 62 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::STATUS_TGL

Status Register

Definition at line 82 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::SYNCBUSY

Syncbusy

Definition at line 55 of file efr32bg21_acmp.h.

Referenced by ACMP_CapsenseChannelSet(), ACMP_ChannelSet(), and ACMP_Disable().

__IM uint32_t ACMP_TypeDef::SYNCBUSY_CLR

Syncbusy

Definition at line 75 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::SYNCBUSY_SET

Syncbusy

Definition at line 65 of file efr32bg21_acmp.h.

__IM uint32_t ACMP_TypeDef::SYNCBUSY_TGL

Syncbusy

Definition at line 85 of file efr32bg21_acmp.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_acmp.h