AES_TypeDef Struct ReferenceDevices > AES

AES Register Declaration.

Definition at line 45 of file efr32bg21_aes.h.

#include <efr32bg21_aes.h>

Data Fields

__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t FETCHADDR
 
__IOM uint32_t FETCHDESCR
 
__IOM uint32_t FETCHLEN
 
__IOM uint32_t FETCHTAG
 
__IOM uint32_t IEN
 
__IM uint32_t IF
 
__IOM uint32_t IFC
 
__IOM uint32_t PUSHADDR
 
__IOM uint32_t PUSHDESCR
 
__IOM uint32_t PUSHLEN
 
uint32_t RESERVED0 [2U]
 
uint32_t RESERVED1 [1U]
 
uint32_t RESERVED2 [4079U]
 
uint32_t RESERVED3 [1U]
 
__IM uint32_t STATUS
 

Field Documentation

__IOM uint32_t AES_TypeDef::CMD

Command register

Definition at line 59 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::CTRL

Control register

Definition at line 58 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::FETCHADDR

Fetcher Address

Definition at line 46 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::FETCHDESCR

Fetcher Descriptor

Definition at line 47 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::FETCHLEN

Fetcher Length

Definition at line 48 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::FETCHTAG

Fetcher Tag

Definition at line 49 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::IEN

Interrupt Enable

Definition at line 53 of file efr32bg21_aes.h.

__IM uint32_t AES_TypeDef::IF

Interrupt Flags

Definition at line 55 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::IFC

Interrupt status clear

Definition at line 57 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::PUSHADDR

Pusher Address

Definition at line 50 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::PUSHDESCR

Pusher Descriptor

Definition at line 51 of file efr32bg21_aes.h.

__IOM uint32_t AES_TypeDef::PUSHLEN

Pusher Length

Definition at line 52 of file efr32bg21_aes.h.

uint32_t AES_TypeDef::RESERVED0[2U]

Reserved for future use

Definition at line 54 of file efr32bg21_aes.h.

uint32_t AES_TypeDef::RESERVED1[1U]

Reserved for future use

Definition at line 56 of file efr32bg21_aes.h.

uint32_t AES_TypeDef::RESERVED2[4079U]

Reserved for future use

Definition at line 61 of file efr32bg21_aes.h.

uint32_t AES_TypeDef::RESERVED3[1U]

Reserved for future use

Definition at line 62 of file efr32bg21_aes.h.

__IM uint32_t AES_TypeDef::STATUS

Status register

Definition at line 60 of file efr32bg21_aes.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_aes.h