AMUXCP_TypeDef Struct ReferenceDevices > AMUXCP

AMUXCP Register Declaration.

Definition at line 46 of file efr32bg21_amuxcp.h.

#include <efr32bg21_amuxcp.h>

Data Fields

__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [1018U]
 
uint32_t RESERVED2 [1U]
 
uint32_t RESERVED3 [1018U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [1018U]
 
uint32_t RESERVED6 [1U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t TEST
 
__IOM uint32_t TEST_CLR
 
__IOM uint32_t TEST_SET
 
__IOM uint32_t TEST_TGL
 
__IOM uint32_t TRIM
 
__IOM uint32_t TRIM_CLR
 
__IOM uint32_t TRIM_SET
 
__IOM uint32_t TRIM_TGL
 

Field Documentation

__IOM uint32_t AMUXCP_TypeDef::CTRL

Control

Definition at line 49 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::CTRL_CLR

Control

Definition at line 63 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::CTRL_SET

Control

Definition at line 56 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::CTRL_TGL

Control

Definition at line 70 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::IPVERSION

IPVERSION

Definition at line 47 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::IPVERSION_CLR

IPVERSION

Definition at line 61 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::IPVERSION_SET

IPVERSION

Definition at line 54 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::IPVERSION_TGL

IPVERSION

Definition at line 68 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 48 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED1[1018U]

Reserved for future use

Definition at line 53 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED2[1U]

Reserved for future use

Definition at line 55 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED3[1018U]

Reserved for future use

Definition at line 60 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 62 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED5[1018U]

Reserved for future use

Definition at line 67 of file efr32bg21_amuxcp.h.

uint32_t AMUXCP_TypeDef::RESERVED6[1U]

Reserved for future use

Definition at line 69 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::STATUS

Status

Definition at line 50 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::STATUS_CLR

Status

Definition at line 64 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::STATUS_SET

Status

Definition at line 57 of file efr32bg21_amuxcp.h.

__IM uint32_t AMUXCP_TypeDef::STATUS_TGL

Status

Definition at line 71 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TEST

Test

Definition at line 51 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TEST_CLR

Test

Definition at line 65 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TEST_SET

Test

Definition at line 58 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TEST_TGL

Test

Definition at line 72 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TRIM

New Register

Definition at line 52 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TRIM_CLR

New Register

Definition at line 66 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TRIM_SET

New Register

Definition at line 59 of file efr32bg21_amuxcp.h.

__IOM uint32_t AMUXCP_TypeDef::TRIM_TGL

New Register

Definition at line 73 of file efr32bg21_amuxcp.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_amuxcp.h