BUFC_BUF_TypeDef Struct ReferenceDevices > BUFC

BUFC BUF Register Group Declaration.

Definition at line 46 of file efr32bg21_bufc.h.

#include <efr32bg21_bufc.h>

Data Fields

__IOM uint32_t ADDR
 
__IOM uint32_t CMD
 
__IOM uint32_t CTRL
 
__IOM uint32_t FIFOASYNC
 
__IM uint32_t READDATA
 
__IOM uint32_t READOFFSET
 
uint32_t RESERVED0 [1U]
 
__IM uint32_t STATUS
 
__IOM uint32_t THRESHOLDCTRL
 
__IOM uint32_t WRITEDATA
 
__IOM uint32_t WRITEOFFSET
 
__IOM uint32_t XWRITE
 

Field Documentation

__IOM uint32_t BUFC_BUF_TypeDef::ADDR

Buffer Address

Definition at line 48 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::CMD

Buffer Command

Definition at line 57 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::CTRL

Buffer Control

Definition at line 47 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::FIFOASYNC

New Register

Definition at line 58 of file efr32bg21_bufc.h.

__IM uint32_t BUFC_BUF_TypeDef::READDATA

Buffer Read Data

Definition at line 52 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::READOFFSET

Read Offset

Definition at line 50 of file efr32bg21_bufc.h.

uint32_t BUFC_BUF_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 51 of file efr32bg21_bufc.h.

__IM uint32_t BUFC_BUF_TypeDef::STATUS

Buffer Status Register

Definition at line 55 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::THRESHOLDCTRL

Threshold Control

Definition at line 56 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::WRITEDATA

Buffer Write Data

Definition at line 53 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::WRITEOFFSET

Write Offset

Definition at line 49 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_BUF_TypeDef::XWRITE

Buffer XOR Write

Definition at line 54 of file efr32bg21_bufc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_bufc.h