BUFC_TypeDef Struct ReferenceDevices > BUFC

BUFC Register Declaration.

Definition at line 62 of file efr32bg21_bufc.h.

#include <efr32bg21_bufc.h>

Data Fields

BUFC_BUF_TypeDef BUF [4U]
 
BUFC_BUF_TypeDef BUF_CLR [4U]
 
BUFC_BUF_TypeDef BUF_SET [4U]
 
BUFC_BUF_TypeDef BUF_TGL [4U]
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t RAMBASEADDR
 
__IOM uint32_t RAMBASEADDR_CLR
 
__IOM uint32_t RAMBASEADDR_SET
 
__IOM uint32_t RAMBASEADDR_TGL
 
uint32_t RESERVED0 [6U]
 
uint32_t RESERVED1 [2U]
 
uint32_t RESERVED10 [2U]
 
uint32_t RESERVED2 [963U]
 
uint32_t RESERVED3 [6U]
 
uint32_t RESERVED4 [2U]
 
uint32_t RESERVED5 [963U]
 
uint32_t RESERVED6 [6U]
 
uint32_t RESERVED7 [2U]
 
uint32_t RESERVED8 [963U]
 
uint32_t RESERVED9 [6U]
 

Field Documentation

BUFC_BUF_TypeDef BUFC_TypeDef::BUF[4U]

Data Buffer

Definition at line 65 of file efr32bg21_bufc.h.

BUFC_BUF_TypeDef BUFC_TypeDef::BUF_CLR[4U]

Data Buffer

Definition at line 83 of file efr32bg21_bufc.h.

BUFC_BUF_TypeDef BUFC_TypeDef::BUF_SET[4U]

Data Buffer

Definition at line 74 of file efr32bg21_bufc.h.

BUFC_BUF_TypeDef BUFC_TypeDef::BUF_TGL[4U]

Data Buffer

Definition at line 92 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::EN

Enable peripheral clock to this module

Definition at line 64 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::EN_CLR

Enable peripheral clock to this module

Definition at line 82 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::EN_SET

Enable peripheral clock to this module

Definition at line 73 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::EN_TGL

Enable peripheral clock to this module

Definition at line 91 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IEN

Interrupt Enable Register

Definition at line 69 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 87 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 78 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 96 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IF

BUFC Interrupt Flags

Definition at line 67 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IF_CLR

BUFC Interrupt Flags

Definition at line 85 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IF_SET

BUFC Interrupt Flags

Definition at line 76 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::IF_TGL

BUFC Interrupt Flags

Definition at line 94 of file efr32bg21_bufc.h.

__IM uint32_t BUFC_TypeDef::IPVERSION

IP Version

Definition at line 63 of file efr32bg21_bufc.h.

__IM uint32_t BUFC_TypeDef::IPVERSION_CLR

IP Version

Definition at line 81 of file efr32bg21_bufc.h.

__IM uint32_t BUFC_TypeDef::IPVERSION_SET

IP Version

Definition at line 72 of file efr32bg21_bufc.h.

__IM uint32_t BUFC_TypeDef::IPVERSION_TGL

IP Version

Definition at line 90 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::RAMBASEADDR

New Register

Definition at line 70 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::RAMBASEADDR_CLR

New Register

Definition at line 88 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::RAMBASEADDR_SET

New Register

Definition at line 79 of file efr32bg21_bufc.h.

__IOM uint32_t BUFC_TypeDef::RAMBASEADDR_TGL

New Register

Definition at line 97 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED0[6U]

Reserved for future use

Definition at line 66 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED1[2U]

Reserved for future use

Definition at line 68 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED10[2U]

Reserved for future use

Definition at line 95 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED2[963U]

Reserved for future use

Definition at line 71 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED3[6U]

Reserved for future use

Definition at line 75 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED4[2U]

Reserved for future use

Definition at line 77 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED5[963U]

Reserved for future use

Definition at line 80 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED6[6U]

Reserved for future use

Definition at line 84 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED7[2U]

Reserved for future use

Definition at line 86 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED8[963U]

Reserved for future use

Definition at line 89 of file efr32bg21_bufc.h.

uint32_t BUFC_TypeDef::RESERVED9[6U]

Reserved for future use

Definition at line 93 of file efr32bg21_bufc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_bufc.h