BURAM_TypeDef Struct ReferenceDevices > BURAM

BURAM Register Declaration.

Definition at line 51 of file efr32bg21_buram.h.

#include <efr32bg21_buram.h>

Data Fields

uint32_t RESERVED0 [992U]
 
uint32_t RESERVED1 [992U]
 
uint32_t RESERVED2 [992U]
 
BURAM_RET_TypeDef RET [32U]
 
BURAM_RET_TypeDef RET_CLR [32U]
 
BURAM_RET_TypeDef RET_SET [32U]
 
BURAM_RET_TypeDef RET_TGL [32U]
 

Field Documentation

uint32_t BURAM_TypeDef::RESERVED0[992U]

Reserved for future use

Definition at line 53 of file efr32bg21_buram.h.

uint32_t BURAM_TypeDef::RESERVED1[992U]

Reserved for future use

Definition at line 55 of file efr32bg21_buram.h.

uint32_t BURAM_TypeDef::RESERVED2[992U]

Reserved for future use

Definition at line 57 of file efr32bg21_buram.h.

BURAM_RET_TypeDef BURAM_TypeDef::RET[32U]

RetentionReg

Definition at line 52 of file efr32bg21_buram.h.

BURAM_RET_TypeDef BURAM_TypeDef::RET_CLR[32U]

RetentionReg

Definition at line 56 of file efr32bg21_buram.h.

BURAM_RET_TypeDef BURAM_TypeDef::RET_SET[32U]

RetentionReg

Definition at line 54 of file efr32bg21_buram.h.

BURAM_RET_TypeDef BURAM_TypeDef::RET_TGL[32U]

RetentionReg

Definition at line 58 of file efr32bg21_buram.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_buram.h