BURTC_TypeDef Struct ReferenceDevices > BURTC

BURTC Register Declaration.

Definition at line 46 of file efr32bg21_burtc.h.

#include <efr32bg21_burtc.h>

Data Fields

__IOM uint32_t CFG
 
__IOM uint32_t CFG_CLR
 
__IOM uint32_t CFG_SET
 
__IOM uint32_t CFG_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CNT
 
__IOM uint32_t CNT_CLR
 
__IOM uint32_t CNT_SET
 
__IOM uint32_t CNT_TGL
 
__IOM uint32_t COMP
 
__IOM uint32_t COMP_CLR
 
__IOM uint32_t COMP_SET
 
__IOM uint32_t COMP_TGL
 
__IOM uint32_t EM4WUEN
 
__IOM uint32_t EM4WUEN_CLR
 
__IOM uint32_t EM4WUEN_SET
 
__IOM uint32_t EM4WUEN_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
__IOM uint32_t PRECNT
 
__IOM uint32_t PRECNT_CLR
 
__IOM uint32_t PRECNT_SET
 
__IOM uint32_t PRECNT_TGL
 
uint32_t RESERVED0 [1011U]
 
uint32_t RESERVED1 [1011U]
 
uint32_t RESERVED2 [1011U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IM uint32_t SYNCBUSY
 
__IM uint32_t SYNCBUSY_CLR
 
__IM uint32_t SYNCBUSY_SET
 
__IM uint32_t SYNCBUSY_TGL
 

Field Documentation

__IOM uint32_t BURTC_TypeDef::CFG

Configuration Register

Definition at line 49 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CFG_CLR

Configuration Register

Definition at line 77 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CFG_SET

Configuration Register

Definition at line 63 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CFG_TGL

Configuration Register

Definition at line 91 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CMD

Command Register

Definition at line 50 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CMD_CLR

Command Register

Definition at line 78 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CMD_SET

Command Register

Definition at line 64 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CMD_TGL

Command Register

Definition at line 92 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CNT

Counter Value Register

Definition at line 55 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CNT_CLR

Counter Value Register

Definition at line 83 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CNT_SET

Counter Value Register

Definition at line 69 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::CNT_TGL

Counter Value Register

Definition at line 97 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::COMP

Compare Value Register

Definition at line 59 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::COMP_CLR

Compare Value Register

Definition at line 87 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::COMP_SET

Compare Value Register

Definition at line 73 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::COMP_TGL

Compare Value Register

Definition at line 101 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EM4WUEN

EM4 wakeup request Enable Register

Definition at line 56 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EM4WUEN_CLR

EM4 wakeup request Enable Register

Definition at line 84 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EM4WUEN_SET

EM4 wakeup request Enable Register

Definition at line 70 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EM4WUEN_TGL

EM4 wakeup request Enable Register

Definition at line 98 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EN

Module Enable Register

Definition at line 48 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EN_CLR

Module Enable Register

Definition at line 76 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EN_SET

Module Enable Register

Definition at line 62 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::EN_TGL

Module Enable Register

Definition at line 90 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IEN

Interrupt Enable Register

Definition at line 53 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 81 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 67 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 95 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IF

Interrupt Flag Register

Definition at line 52 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 80 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 66 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 94 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::IPVERSION

IP version ID

Definition at line 47 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::IPVERSION_CLR

IP version ID

Definition at line 75 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::IPVERSION_SET

IP version ID

Definition at line 61 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::IPVERSION_TGL

IP version ID

Definition at line 89 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::LOCK

Configuration Lock Register

Definition at line 58 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::LOCK_CLR

Configuration Lock Register

Definition at line 86 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::LOCK_SET

Configuration Lock Register

Definition at line 72 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::LOCK_TGL

Configuration Lock Register

Definition at line 100 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::PRECNT

Pre-Counter Value Register

Definition at line 54 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::PRECNT_CLR

Pre-Counter Value Register

Definition at line 82 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::PRECNT_SET

Pre-Counter Value Register

Definition at line 68 of file efr32bg21_burtc.h.

__IOM uint32_t BURTC_TypeDef::PRECNT_TGL

Pre-Counter Value Register

Definition at line 96 of file efr32bg21_burtc.h.

uint32_t BURTC_TypeDef::RESERVED0[1011U]

Reserved for future use

Definition at line 60 of file efr32bg21_burtc.h.

uint32_t BURTC_TypeDef::RESERVED1[1011U]

Reserved for future use

Definition at line 74 of file efr32bg21_burtc.h.

uint32_t BURTC_TypeDef::RESERVED2[1011U]

Reserved for future use

Definition at line 88 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::STATUS

Status Register

Definition at line 51 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::STATUS_CLR

Status Register

Definition at line 79 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::STATUS_SET

Status Register

Definition at line 65 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::STATUS_TGL

Status Register

Definition at line 93 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::SYNCBUSY

Synchronization Busy Register

Definition at line 57 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::SYNCBUSY_CLR

Synchronization Busy Register

Definition at line 85 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::SYNCBUSY_SET

Synchronization Busy Register

Definition at line 71 of file efr32bg21_burtc.h.

__IM uint32_t BURTC_TypeDef::SYNCBUSY_TGL

Synchronization Busy Register

Definition at line 99 of file efr32bg21_burtc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_burtc.h