CMU_TypeDef Struct ReferenceDevices > CMU

CMU Register Declaration.

Definition at line 46 of file efr32bg21_cmu.h.

#include <efr32bg21_cmu.h>

Data Fields

__IOM uint32_t CALCMD
 
__IOM uint32_t CALCMD_CLR
 
__IOM uint32_t CALCMD_SET
 
__IOM uint32_t CALCMD_TGL
 
__IM uint32_t CALCNT
 
__IM uint32_t CALCNT_CLR
 
__IM uint32_t CALCNT_SET
 
__IM uint32_t CALCNT_TGL
 
__IOM uint32_t CALCTRL
 
__IOM uint32_t CALCTRL_CLR
 
__IOM uint32_t CALCTRL_SET
 
__IOM uint32_t CALCTRL_TGL
 
__IOM uint32_t DPLLREFCLKCTRL
 
__IOM uint32_t DPLLREFCLKCTRL_CLR
 
__IOM uint32_t DPLLREFCLKCTRL_SET
 
__IOM uint32_t DPLLREFCLKCTRL_TGL
 
__IOM uint32_t EM01GRPACLKCTRL
 
__IOM uint32_t EM01GRPACLKCTRL_CLR
 
__IOM uint32_t EM01GRPACLKCTRL_SET
 
__IOM uint32_t EM01GRPACLKCTRL_TGL
 
__IOM uint32_t EM23GRPACLKCTRL
 
__IOM uint32_t EM23GRPACLKCTRL_CLR
 
__IOM uint32_t EM23GRPACLKCTRL_SET
 
__IOM uint32_t EM23GRPACLKCTRL_TGL
 
__IOM uint32_t EM4GRPACLKCTRL
 
__IOM uint32_t EM4GRPACLKCTRL_CLR
 
__IOM uint32_t EM4GRPACLKCTRL_SET
 
__IOM uint32_t EM4GRPACLKCTRL_TGL
 
__IOM uint32_t EXPORTCLKCTRL
 
__IOM uint32_t EXPORTCLKCTRL_CLR
 
__IOM uint32_t EXPORTCLKCTRL_SET
 
__IOM uint32_t EXPORTCLKCTRL_TGL
 
__IOM uint32_t IADCCLKCTRL
 
__IOM uint32_t IADCCLKCTRL_CLR
 
__IOM uint32_t IADCCLKCTRL_SET
 
__IOM uint32_t IADCCLKCTRL_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
__IOM uint32_t RADIOCLKCTRL
 
__IOM uint32_t RADIOCLKCTRL_CLR
 
__IOM uint32_t RADIOCLKCTRL_SET
 
__IOM uint32_t RADIOCLKCTRL_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [1U]
 
uint32_t RESERVED10 [7U]
 
uint32_t RESERVED11 [7U]
 
uint32_t RESERVED12 [31U]
 
uint32_t RESERVED13 [1U]
 
uint32_t RESERVED14 [13U]
 
uint32_t RESERVED15 [15U]
 
uint32_t RESERVED16 [863U]
 
uint32_t RESERVED17 [1U]
 
uint32_t RESERVED18 [1U]
 
uint32_t RESERVED19 [2U]
 
uint32_t RESERVED2 [2U]
 
uint32_t RESERVED20 [10U]
 
uint32_t RESERVED21 [5U]
 
uint32_t RESERVED22 [3U]
 
uint32_t RESERVED23 [3U]
 
uint32_t RESERVED24 [27U]
 
uint32_t RESERVED25 [7U]
 
uint32_t RESERVED26 [7U]
 
uint32_t RESERVED27 [7U]
 
uint32_t RESERVED28 [7U]
 
uint32_t RESERVED29 [31U]
 
uint32_t RESERVED3 [10U]
 
uint32_t RESERVED30 [1U]
 
uint32_t RESERVED31 [13U]
 
uint32_t RESERVED32 [15U]
 
uint32_t RESERVED33 [863U]
 
uint32_t RESERVED34 [1U]
 
uint32_t RESERVED35 [1U]
 
uint32_t RESERVED36 [2U]
 
uint32_t RESERVED37 [10U]
 
uint32_t RESERVED38 [5U]
 
uint32_t RESERVED39 [3U]
 
uint32_t RESERVED4 [5U]
 
uint32_t RESERVED40 [3U]
 
uint32_t RESERVED41 [27U]
 
uint32_t RESERVED42 [7U]
 
uint32_t RESERVED43 [7U]
 
uint32_t RESERVED44 [7U]
 
uint32_t RESERVED45 [7U]
 
uint32_t RESERVED46 [31U]
 
uint32_t RESERVED47 [1U]
 
uint32_t RESERVED48 [13U]
 
uint32_t RESERVED49 [15U]
 
uint32_t RESERVED5 [3U]
 
uint32_t RESERVED50 [863U]
 
uint32_t RESERVED51 [1U]
 
uint32_t RESERVED52 [1U]
 
uint32_t RESERVED53 [2U]
 
uint32_t RESERVED54 [10U]
 
uint32_t RESERVED55 [5U]
 
uint32_t RESERVED56 [3U]
 
uint32_t RESERVED57 [3U]
 
uint32_t RESERVED58 [27U]
 
uint32_t RESERVED59 [7U]
 
uint32_t RESERVED6 [3U]
 
uint32_t RESERVED60 [7U]
 
uint32_t RESERVED61 [7U]
 
uint32_t RESERVED62 [7U]
 
uint32_t RESERVED63 [31U]
 
uint32_t RESERVED64 [1U]
 
uint32_t RESERVED65 [13U]
 
uint32_t RESERVED66 [15U]
 
uint32_t RESERVED7 [27U]
 
uint32_t RESERVED8 [7U]
 
uint32_t RESERVED9 [7U]
 
__IOM uint32_t RTCCCLKCTRL
 
__IOM uint32_t RTCCCLKCTRL_CLR
 
__IOM uint32_t RTCCCLKCTRL_SET
 
__IOM uint32_t RTCCCLKCTRL_TGL
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t SYSCLKCTRL
 
__IOM uint32_t SYSCLKCTRL_CLR
 
__IOM uint32_t SYSCLKCTRL_SET
 
__IOM uint32_t SYSCLKCTRL_TGL
 
__IOM uint32_t TRACECLKCTRL
 
__IOM uint32_t TRACECLKCTRL_CLR
 
__IOM uint32_t TRACECLKCTRL_SET
 
__IOM uint32_t TRACECLKCTRL_TGL
 
__IOM uint32_t WDOG0CLKCTRL
 
__IOM uint32_t WDOG0CLKCTRL_CLR
 
__IOM uint32_t WDOG0CLKCTRL_SET
 
__IOM uint32_t WDOG0CLKCTRL_TGL
 
__IOM uint32_t WDOG1CLKCTRL
 
__IOM uint32_t WDOG1CLKCTRL_CLR
 
__IOM uint32_t WDOG1CLKCTRL_SET
 
__IOM uint32_t WDOG1CLKCTRL_TGL
 
__IOM uint32_t WDOGLOCK
 
__IOM uint32_t WDOGLOCK_CLR
 
__IOM uint32_t WDOGLOCK_SET
 
__IOM uint32_t WDOGLOCK_TGL
 

Field Documentation

__IOM uint32_t CMU_TypeDef::CALCMD

Calibration Command Register

Definition at line 57 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCMD_CLR

Calibration Command Register

Definition at line 133 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCMD_SET

Calibration Command Register

Definition at line 95 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCMD_TGL

Calibration Command Register

Definition at line 171 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::CALCNT

Calibration Result Counter Register

Definition at line 59 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::CALCNT_CLR

Calibration Result Counter Register

Definition at line 135 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::CALCNT_SET

Calibration Result Counter Register

Definition at line 97 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::CALCNT_TGL

Calibration Result Counter Register

Definition at line 173 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCTRL

Calibration Control Register

Definition at line 58 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCTRL_CLR

Calibration Control Register

Definition at line 134 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCTRL_SET

Calibration Control Register

Definition at line 96 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::CALCTRL_TGL

Calibration Control Register

Definition at line 172 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::DPLLREFCLKCTRL

Digital PLL Reference Clock Control

Definition at line 67 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::DPLLREFCLKCTRL_CLR

Digital PLL Reference Clock Control

Definition at line 143 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::DPLLREFCLKCTRL_SET

Digital PLL Reference Clock Control

Definition at line 105 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::DPLLREFCLKCTRL_TGL

Digital PLL Reference Clock Control

Definition at line 181 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM01GRPACLKCTRL

EM01 Peripheral Group A Clock Control

Definition at line 69 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM01GRPACLKCTRL_CLR

EM01 Peripheral Group A Clock Control

Definition at line 145 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM01GRPACLKCTRL_SET

EM01 Peripheral Group A Clock Control

Definition at line 107 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM01GRPACLKCTRL_TGL

EM01 Peripheral Group A Clock Control

Definition at line 183 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM23GRPACLKCTRL

EM23 Peripheral Group A Clock Control

Definition at line 71 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM23GRPACLKCTRL_CLR

EM23 Peripheral Group A Clock Control

Definition at line 147 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM23GRPACLKCTRL_SET

EM23 Peripheral Group A Clock Control

Definition at line 109 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM23GRPACLKCTRL_TGL

EM23 Peripheral Group A Clock Control

Definition at line 185 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM4GRPACLKCTRL

EM4 Peripheral Group A Clock Control

Definition at line 73 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM4GRPACLKCTRL_CLR

EM4 Peripheral Group A Clock Control

Definition at line 149 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM4GRPACLKCTRL_SET

EM4 Peripheral Group A Clock Control

Definition at line 111 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EM4GRPACLKCTRL_TGL

EM4 Peripheral Group A Clock Control

Definition at line 187 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EXPORTCLKCTRL

Export Clock Control

Definition at line 65 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EXPORTCLKCTRL_CLR

Export Clock Control

Definition at line 141 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EXPORTCLKCTRL_SET

Export Clock Control

Definition at line 103 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::EXPORTCLKCTRL_TGL

Export Clock Control

Definition at line 179 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IADCCLKCTRL

IADC Clock Control

Definition at line 75 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IADCCLKCTRL_CLR

IADC Clock Control

Definition at line 151 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IADCCLKCTRL_SET

IADC Clock Control

Definition at line 113 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IADCCLKCTRL_TGL

IADC Clock Control

Definition at line 189 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IEN

Interrupt Enable Register

Definition at line 55 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 131 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 93 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 169 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IF

Interrupt Flag Register

Definition at line 54 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 130 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 92 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 168 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::IPVERSION

IP version ID

Definition at line 47 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::IPVERSION_CLR

IP version ID

Definition at line 123 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::IPVERSION_SET

IP version ID

Definition at line 85 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::IPVERSION_TGL

IP version ID

Definition at line 161 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::LOCK

Configuration Lock Register

Definition at line 51 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::LOCK_CLR

Configuration Lock Register

Definition at line 127 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::LOCK_SET

Configuration Lock Register

Definition at line 89 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::LOCK_TGL

Configuration Lock Register

Definition at line 165 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RADIOCLKCTRL

Radio Clock Control

Definition at line 83 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RADIOCLKCTRL_CLR

Radio Clock Control

Definition at line 159 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RADIOCLKCTRL_SET

Radio Clock Control

Definition at line 121 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RADIOCLKCTRL_TGL

Radio Clock Control

Definition at line 197 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 48 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED1[1U]

Reserved for future use

Definition at line 50 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED10[7U]

Reserved for future use

Definition at line 72 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED11[7U]

Reserved for future use

Definition at line 74 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED12[31U]

Reserved for future use

Definition at line 76 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED13[1U]

Reserved for future use

Definition at line 78 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED14[13U]

Reserved for future use

Definition at line 80 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED15[15U]

Reserved for future use

Definition at line 82 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED16[863U]

Reserved for future use

Definition at line 84 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED17[1U]

Reserved for future use

Definition at line 86 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED18[1U]

Reserved for future use

Definition at line 88 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED19[2U]

Reserved for future use

Definition at line 91 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED2[2U]

Reserved for future use

Definition at line 53 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED20[10U]

Reserved for future use

Definition at line 94 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED21[5U]

Reserved for future use

Definition at line 98 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED22[3U]

Reserved for future use

Definition at line 100 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED23[3U]

Reserved for future use

Definition at line 102 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED24[27U]

Reserved for future use

Definition at line 104 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED25[7U]

Reserved for future use

Definition at line 106 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED26[7U]

Reserved for future use

Definition at line 108 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED27[7U]

Reserved for future use

Definition at line 110 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED28[7U]

Reserved for future use

Definition at line 112 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED29[31U]

Reserved for future use

Definition at line 114 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED3[10U]

Reserved for future use

Definition at line 56 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED30[1U]

Reserved for future use

Definition at line 116 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED31[13U]

Reserved for future use

Definition at line 118 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED32[15U]

Reserved for future use

Definition at line 120 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED33[863U]

Reserved for future use

Definition at line 122 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED34[1U]

Reserved for future use

Definition at line 124 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED35[1U]

Reserved for future use

Definition at line 126 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED36[2U]

Reserved for future use

Definition at line 129 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED37[10U]

Reserved for future use

Definition at line 132 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED38[5U]

Reserved for future use

Definition at line 136 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED39[3U]

Reserved for future use

Definition at line 138 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED4[5U]

Reserved for future use

Definition at line 60 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED40[3U]

Reserved for future use

Definition at line 140 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED41[27U]

Reserved for future use

Definition at line 142 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED42[7U]

Reserved for future use

Definition at line 144 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED43[7U]

Reserved for future use

Definition at line 146 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED44[7U]

Reserved for future use

Definition at line 148 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED45[7U]

Reserved for future use

Definition at line 150 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED46[31U]

Reserved for future use

Definition at line 152 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED47[1U]

Reserved for future use

Definition at line 154 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED48[13U]

Reserved for future use

Definition at line 156 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED49[15U]

Reserved for future use

Definition at line 158 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED5[3U]

Reserved for future use

Definition at line 62 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED50[863U]

Reserved for future use

Definition at line 160 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED51[1U]

Reserved for future use

Definition at line 162 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED52[1U]

Reserved for future use

Definition at line 164 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED53[2U]

Reserved for future use

Definition at line 167 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED54[10U]

Reserved for future use

Definition at line 170 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED55[5U]

Reserved for future use

Definition at line 174 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED56[3U]

Reserved for future use

Definition at line 176 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED57[3U]

Reserved for future use

Definition at line 178 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED58[27U]

Reserved for future use

Definition at line 180 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED59[7U]

Reserved for future use

Definition at line 182 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED6[3U]

Reserved for future use

Definition at line 64 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED60[7U]

Reserved for future use

Definition at line 184 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED61[7U]

Reserved for future use

Definition at line 186 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED62[7U]

Reserved for future use

Definition at line 188 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED63[31U]

Reserved for future use

Definition at line 190 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED64[1U]

Reserved for future use

Definition at line 192 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED65[13U]

Reserved for future use

Definition at line 194 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED66[15U]

Reserved for future use

Definition at line 196 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED7[27U]

Reserved for future use

Definition at line 66 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED8[7U]

Reserved for future use

Definition at line 68 of file efr32bg21_cmu.h.

uint32_t CMU_TypeDef::RESERVED9[7U]

Reserved for future use

Definition at line 70 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RTCCCLKCTRL

RTCC Clock Control

Definition at line 81 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RTCCCLKCTRL_CLR

RTCC Clock Control

Definition at line 157 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RTCCCLKCTRL_SET

RTCC Clock Control

Definition at line 119 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::RTCCCLKCTRL_TGL

RTCC Clock Control

Definition at line 195 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::STATUS

Status Register

Definition at line 49 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::STATUS_CLR

Status Register

Definition at line 125 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::STATUS_SET

Status Register

Definition at line 87 of file efr32bg21_cmu.h.

__IM uint32_t CMU_TypeDef::STATUS_TGL

Status Register

Definition at line 163 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::SYSCLKCTRL

System Clock Control

Definition at line 61 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::SYSCLKCTRL_CLR

System Clock Control

Definition at line 137 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::SYSCLKCTRL_SET

System Clock Control

Definition at line 99 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::SYSCLKCTRL_TGL

System Clock Control

Definition at line 175 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::TRACECLKCTRL

Debug Trace Clock Control

Definition at line 63 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::TRACECLKCTRL_CLR

Debug Trace Clock Control

Definition at line 139 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::TRACECLKCTRL_SET

Debug Trace Clock Control

Definition at line 101 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::TRACECLKCTRL_TGL

Debug Trace Clock Control

Definition at line 177 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG0CLKCTRL

Watchdog0 Clock Control

Definition at line 77 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG0CLKCTRL_CLR

Watchdog0 Clock Control

Definition at line 153 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG0CLKCTRL_SET

Watchdog0 Clock Control

Definition at line 115 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG0CLKCTRL_TGL

Watchdog0 Clock Control

Definition at line 191 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG1CLKCTRL

Watchdog1 Clock Control

Definition at line 79 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG1CLKCTRL_CLR

Watchdog1 Clock Control

Definition at line 155 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG1CLKCTRL_SET

Watchdog1 Clock Control

Definition at line 117 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOG1CLKCTRL_TGL

Watchdog1 Clock Control

Definition at line 193 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOGLOCK

WDOG Configuration Lock Register

Definition at line 52 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOGLOCK_CLR

WDOG Configuration Lock Register

Definition at line 128 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOGLOCK_SET

WDOG Configuration Lock Register

Definition at line 90 of file efr32bg21_cmu.h.

__IOM uint32_t CMU_TypeDef::WDOGLOCK_TGL

WDOG Configuration Lock Register

Definition at line 166 of file efr32bg21_cmu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_cmu.h