DEVINFO_HFRCODPLLCAL_TypeDef Struct ReferenceDevices > DEVINFO

DEVINFO HFRCODPLLCAL Register Group Declaration.

Definition at line 45 of file efr32bg21_devinfo.h.

#include <efr32bg21_devinfo.h>

Data Fields

__IM uint32_t HFRCODPLLCAL
 

Field Documentation

__IM uint32_t DEVINFO_HFRCODPLLCAL_TypeDef::HFRCODPLLCAL

HFRCODPLL Calibration

Definition at line 46 of file efr32bg21_devinfo.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_devinfo.h