DEVINFO_HFRCOSECAL_TypeDef Struct ReferenceDevices > DEVINFO

DEVINFO HFRCOSECAL Register Group Declaration.

Definition at line 55 of file efr32bg21_devinfo.h.

#include <efr32bg21_devinfo.h>

Data Fields

uint32_t RESERVED0 [1U]
 

Field Documentation

uint32_t DEVINFO_HFRCOSECAL_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 56 of file efr32bg21_devinfo.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_devinfo.h