DEVINFO_TypeDef Struct ReferenceDevices > DEVINFO

DEVINFO Register Declaration.

Definition at line 60 of file efr32bg21_devinfo.h.

#include <efr32bg21_devinfo.h>

Data Fields

__IM uint32_t CALTEMP
 
__IM uint32_t CUSTOMINFO
 
__IM uint32_t EMUTEMP
 
__IM uint32_t EUI48H
 
__IM uint32_t EUI48L
 
__IM uint32_t EUI64H
 
__IM uint32_t EUI64L
 
__IM uint32_t EXTINFO
 
DEVINFO_HFRCODPLLCAL_TypeDef HFRCODPLLCAL [18U]
 
DEVINFO_HFRCOEM23CAL_TypeDef HFRCOEM23CAL [18U]
 
DEVINFO_HFRCOSECAL_TypeDef HFRCOSECAL [18U]
 
__IM uint32_t IADC0GAIN0
 
__IM uint32_t IADC0GAIN1
 
__IM uint32_t IADC0HISPDOFFSETCAL0
 
__IM uint32_t IADC0HISPDOFFSETCAL1
 
__IM uint32_t IADC0NORMALOFFSETCAL0
 
__IM uint32_t IADC0NORMALOFFSETCAL1
 
__IM uint32_t IADC0OFFSETCAL0
 
__IM uint32_t INFO
 
__IM uint32_t LEGACY
 
__IM uint32_t MEMINFO
 
__IM uint32_t MODULEINFO
 
__IM uint32_t MODULENAME0
 
__IM uint32_t MODULENAME1
 
__IM uint32_t MODULENAME2
 
__IM uint32_t MODULENAME3
 
__IM uint32_t MODULENAME4
 
__IM uint32_t MODULENAME5
 
__IM uint32_t MODULENAME6
 
__IM uint32_t MODXOCAL
 
__IM uint32_t MSIZE
 
__IM uint32_t PART
 
__IM uint32_t PKGINFO
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [2U]
 
uint32_t RESERVED2 [3U]
 
uint32_t RESERVED3 [11U]
 
uint32_t RESERVED4 [24U]
 
uint32_t RESERVED5 [1U]
 
uint32_t RESERVED6 [103U]
 
uint32_t RESERVED7 [1U]
 
__IM uint32_t SWCAPA0
 
__IM uint32_t SWCAPA1
 
__IM uint32_t SWFIX
 

Field Documentation

__IM uint32_t DEVINFO_TypeDef::CALTEMP

Calibration temperature Information

Definition at line 78 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::CUSTOMINFO

Custom Part Info

Definition at line 66 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::EMUTEMP

EMU Temperature Sensor Calibration Information

Definition at line 79 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::EUI48H

EUI 48 High

Definition at line 75 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::EUI48L

EUI 48 Low

Definition at line 74 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::EUI64H

EUI64 High

Definition at line 77 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::EUI64L

EUI64 Low

Definition at line 76 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::EXTINFO

External Component Info

Definition at line 71 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0GAIN0

IADC Gain Calibration

Definition at line 93 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0GAIN1

IADC Gain Calibration

Definition at line 94 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0HISPDOFFSETCAL0

IADC Offset Calibration

Definition at line 98 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0HISPDOFFSETCAL1

IADC Offset Calibration

Definition at line 99 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0NORMALOFFSETCAL0

IADC Offset Calibration

Definition at line 96 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0NORMALOFFSETCAL1

IADC Offset Calibration

Definition at line 97 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::IADC0OFFSETCAL0

IADC Offset Calibration

Definition at line 95 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::INFO

DI Information

Definition at line 61 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::LEGACY

Legacy Device Info

Definition at line 101 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MEMINFO

Memory Info

Definition at line 63 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULEINFO

Module Information

Definition at line 90 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME0

Module Name Information

Definition at line 83 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME1

Module Name Information

Definition at line 84 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME2

Module Name Information

Definition at line 85 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME3

Module Name Information

Definition at line 86 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME4

Module Name Information

Definition at line 87 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME5

Module Name Information

Definition at line 88 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODULENAME6

Module Name Information

Definition at line 89 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MODXOCAL

Module External Oscillator Calibration Information

Definition at line 91 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::MSIZE

Memory Size

Definition at line 64 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::PART

Part Info

Definition at line 62 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::PKGINFO

Misc Device Info

Definition at line 65 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 70 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED1[2U]

Reserved for future use

Definition at line 72 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED2[3U]

Reserved for future use

Definition at line 73 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED3[11U]

Reserved for future use

Definition at line 92 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED4[24U]

Reserved for future use

Definition at line 100 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED5[1U]

Reserved for future use

Definition at line 102 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED6[103U]

Reserved for future use

Definition at line 103 of file efr32bg21_devinfo.h.

uint32_t DEVINFO_TypeDef::RESERVED7[1U]

Reserved for future use

Definition at line 104 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::SWCAPA0

Software Restriction

Definition at line 68 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::SWCAPA1

Software Restriction

Definition at line 69 of file efr32bg21_devinfo.h.

__IM uint32_t DEVINFO_TypeDef::SWFIX

SW Fix Register

Definition at line 67 of file efr32bg21_devinfo.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_devinfo.h