EMU_TypeDef Struct ReferenceDevices > EMU

EMU Register Declaration.

Definition at line 46 of file efr32bg21_emu.h.

#include <efr32bg21_emu.h>

Data Fields

__IOM uint32_t BOD3SENSE
 
__IOM uint32_t BOD3SENSE_CLR
 
__IOM uint32_t BOD3SENSE_SET
 
__IOM uint32_t BOD3SENSE_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t DECBOD
 
__IOM uint32_t DECBOD_CLR
 
__IOM uint32_t DECBOD_SET
 
__IOM uint32_t DECBOD_TGL
 
__IOM uint32_t DGIEN
 
__IOM uint32_t DGIEN_CLR
 
__IOM uint32_t DGIEN_SET
 
__IOM uint32_t DGIEN_TGL
 
__IOM uint32_t DGIF
 
__IOM uint32_t DGIF_CLR
 
__IOM uint32_t DGIF_SET
 
__IOM uint32_t DGIF_TGL
 
__IOM uint32_t EM4CTRL
 
__IOM uint32_t EM4CTRL_CLR
 
__IOM uint32_t EM4CTRL_SET
 
__IOM uint32_t EM4CTRL_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
uint32_t RESERVED0 [4U]
 
uint32_t RESERVED1 [3U]
 
uint32_t RESERVED10 [3U]
 
uint32_t RESERVED11 [15U]
 
uint32_t RESERVED12 [2U]
 
uint32_t RESERVED13 [1U]
 
uint32_t RESERVED14 [2U]
 
uint32_t RESERVED15 [4U]
 
uint32_t RESERVED16 [1U]
 
uint32_t RESERVED17 [975U]
 
uint32_t RESERVED18 [4U]
 
uint32_t RESERVED19 [3U]
 
uint32_t RESERVED2 [15U]
 
uint32_t RESERVED20 [15U]
 
uint32_t RESERVED21 [2U]
 
uint32_t RESERVED22 [1U]
 
uint32_t RESERVED23 [2U]
 
uint32_t RESERVED24 [4U]
 
uint32_t RESERVED25 [1U]
 
uint32_t RESERVED26 [975U]
 
uint32_t RESERVED27 [4U]
 
uint32_t RESERVED28 [3U]
 
uint32_t RESERVED29 [15U]
 
uint32_t RESERVED3 [2U]
 
uint32_t RESERVED30 [2U]
 
uint32_t RESERVED31 [1U]
 
uint32_t RESERVED32 [2U]
 
uint32_t RESERVED33 [4U]
 
uint32_t RESERVED34 [1U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [2U]
 
uint32_t RESERVED6 [4U]
 
uint32_t RESERVED7 [1U]
 
uint32_t RESERVED8 [975U]
 
uint32_t RESERVED9 [4U]
 
__IM uint32_t RSTCAUSE
 
__IM uint32_t RSTCAUSE_CLR
 
__IM uint32_t RSTCAUSE_SET
 
__IM uint32_t RSTCAUSE_TGL
 
__IOM uint32_t RSTCTRL
 
__IOM uint32_t RSTCTRL_CLR
 
__IOM uint32_t RSTCTRL_SET
 
__IOM uint32_t RSTCTRL_TGL
 
__IOM uint32_t SEIEN
 
__IOM uint32_t SEIEN_CLR
 
__IOM uint32_t SEIEN_SET
 
__IOM uint32_t SEIEN_TGL
 
__IOM uint32_t SEIF
 
__IOM uint32_t SEIF_CLR
 
__IOM uint32_t SEIF_SET
 
__IOM uint32_t SEIF_TGL
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IM uint32_t TEMP
 
__IM uint32_t TEMP_CLR
 
__IM uint32_t TEMP_SET
 
__IM uint32_t TEMP_TGL
 
__IOM uint32_t TEMPLIMITS
 
__IOM uint32_t TEMPLIMITS_CLR
 
__IOM uint32_t TEMPLIMITS_SET
 
__IOM uint32_t TEMPLIMITS_TGL
 

Field Documentation

__IOM uint32_t EMU_TypeDef::BOD3SENSE

BOD3SENSE Control register

Definition at line 50 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::BOD3SENSE_CLR

BOD3SENSE Control register

Definition at line 102 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::BOD3SENSE_SET

BOD3SENSE Control register

Definition at line 76 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::BOD3SENSE_TGL

BOD3SENSE Control register

Definition at line 128 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CMD

EMU Command register

Definition at line 56 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CMD_CLR

EMU Command register

Definition at line 108 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CMD_SET

EMU Command register

Definition at line 82 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CMD_TGL

EMU Command register

Definition at line 134 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CTRL

EMU Control register

Definition at line 57 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CTRL_CLR

EMU Control register

Definition at line 109 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CTRL_SET

EMU Control register

Definition at line 83 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::CTRL_TGL

EMU Control register

Definition at line 135 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DECBOD

DECOUPLE LVBOD Control register

Definition at line 48 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DECBOD_CLR

DECOUPLE LVBOD Control register

Definition at line 100 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DECBOD_SET

DECOUPLE LVBOD Control register

Definition at line 74 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DECBOD_TGL

DECOUPLE LVBOD Control register

Definition at line 126 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIEN

Interrupt Enables Debug

Definition at line 67 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIEN_CLR

Interrupt Enables Debug

Definition at line 119 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIEN_SET

Interrupt Enables Debug

Definition at line 93 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIEN_TGL

Interrupt Enables Debug

Definition at line 145 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIF

Interrupt Flags Debug

Definition at line 66 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIF_CLR

Interrupt Flags Debug

Definition at line 118 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIF_SET

Interrupt Flags Debug

Definition at line 92 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::DGIF_TGL

Interrupt Flags Debug

Definition at line 144 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::EM4CTRL

EM4 Control

Definition at line 55 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::EM4CTRL_CLR

EM4 Control

Definition at line 107 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::EM4CTRL_SET

EM4 Control

Definition at line 81 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::EM4CTRL_TGL

EM4 Control

Definition at line 133 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IEN

Interrupt Enables

Definition at line 54 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IEN_CLR

Interrupt Enables

Definition at line 106 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IEN_SET

Interrupt Enables

Definition at line 80 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IEN_TGL

Interrupt Enables

Definition at line 132 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IF

Interrupt Flags

Definition at line 53 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IF_CLR

Interrupt Flags

Definition at line 105 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IF_SET

Interrupt Flags

Definition at line 79 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::IF_TGL

Interrupt Flags

Definition at line 131 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::LOCK

EMU Configuration lock register

Definition at line 52 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::LOCK_CLR

EMU Configuration lock register

Definition at line 104 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::LOCK_SET

EMU Configuration lock register

Definition at line 78 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::LOCK_TGL

EMU Configuration lock register

Definition at line 130 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED0[4U]

Reserved for future use

Definition at line 47 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED1[3U]

Reserved for future use

Definition at line 49 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED10[3U]

Reserved for future use

Definition at line 75 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED11[15U]

Reserved for future use

Definition at line 77 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED12[2U]

Reserved for future use

Definition at line 85 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED13[1U]

Reserved for future use

Definition at line 88 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED14[2U]

Reserved for future use

Definition at line 91 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED15[4U]

Reserved for future use

Definition at line 96 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED16[1U]

Reserved for future use

Definition at line 97 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED17[975U]

Reserved for future use

Definition at line 98 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED18[4U]

Reserved for future use

Definition at line 99 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED19[3U]

Reserved for future use

Definition at line 101 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED2[15U]

Reserved for future use

Definition at line 51 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED20[15U]

Reserved for future use

Definition at line 103 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED21[2U]

Reserved for future use

Definition at line 111 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED22[1U]

Reserved for future use

Definition at line 114 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED23[2U]

Reserved for future use

Definition at line 117 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED24[4U]

Reserved for future use

Definition at line 122 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED25[1U]

Reserved for future use

Definition at line 123 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED26[975U]

Reserved for future use

Definition at line 124 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED27[4U]

Reserved for future use

Definition at line 125 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED28[3U]

Reserved for future use

Definition at line 127 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED29[15U]

Reserved for future use

Definition at line 129 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED3[2U]

Reserved for future use

Definition at line 59 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED30[2U]

Reserved for future use

Definition at line 137 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED31[1U]

Reserved for future use

Definition at line 140 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED32[2U]

Reserved for future use

Definition at line 143 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED33[4U]

Reserved for future use

Definition at line 148 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED34[1U]

Reserved for future use

Definition at line 149 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 62 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED5[2U]

Reserved for future use

Definition at line 65 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED6[4U]

Reserved for future use

Definition at line 70 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED7[1U]

Reserved for future use

Definition at line 71 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED8[975U]

Reserved for future use

Definition at line 72 of file efr32bg21_emu.h.

uint32_t EMU_TypeDef::RESERVED9[4U]

Reserved for future use

Definition at line 73 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::RSTCAUSE

Reset cause

Definition at line 64 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::RSTCAUSE_CLR

Reset cause

Definition at line 116 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::RSTCAUSE_SET

Reset cause

Definition at line 90 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::RSTCAUSE_TGL

Reset cause

Definition at line 142 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::RSTCTRL

Reset Management Control register

Definition at line 63 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::RSTCTRL_CLR

Reset Management Control register

Definition at line 115 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::RSTCTRL_SET

Reset Management Control register

Definition at line 89 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::RSTCTRL_TGL

Reset Management Control register

Definition at line 141 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIEN

Interrupt Enables Secure Elements

Definition at line 69 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIEN_CLR

Interrupt Enables Secure Elements

Definition at line 121 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIEN_SET

Interrupt Enables Secure Elements

Definition at line 95 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIEN_TGL

Interrupt Enables Secure Elements

Definition at line 147 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIF

Interrupt Flags Secure Element

Definition at line 68 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIF_CLR

Interrupt Flags Secure Element

Definition at line 120 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIF_SET

Interrupt Flags Secure Element

Definition at line 94 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::SEIF_TGL

Interrupt Flags Secure Element

Definition at line 146 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::STATUS

EMU Status register

Definition at line 60 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::STATUS_CLR

EMU Status register

Definition at line 112 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::STATUS_SET

EMU Status register

Definition at line 86 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::STATUS_TGL

EMU Status register

Definition at line 138 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::TEMP

Temperature

Definition at line 61 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::TEMP_CLR

Temperature

Definition at line 113 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::TEMP_SET

Temperature

Definition at line 87 of file efr32bg21_emu.h.

__IM uint32_t EMU_TypeDef::TEMP_TGL

Temperature

Definition at line 139 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::TEMPLIMITS

EMU Temperature thresholds

Definition at line 58 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::TEMPLIMITS_CLR

EMU Temperature thresholds

Definition at line 110 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::TEMPLIMITS_SET

EMU Temperature thresholds

Definition at line 84 of file efr32bg21_emu.h.

__IOM uint32_t EMU_TypeDef::TEMPLIMITS_TGL

EMU Temperature thresholds

Definition at line 136 of file efr32bg21_emu.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_emu.h