FRC_TypeDef Struct ReferenceDevices > FRC

FRC Register Declaration.

Definition at line 56 of file efr32bg21_frc.h.

#include <efr32bg21_frc.h>

Data Fields

__IOM uint32_t ADDRFILTCTRL
 
__IOM uint32_t ADDRFILTCTRL_CLR
 
__IOM uint32_t ADDRFILTCTRL_SET
 
__IOM uint32_t ADDRFILTCTRL_TGL
 
__IOM uint32_t AUTOCG
 
__IOM uint32_t AUTOCG_CLR
 
__IOM uint32_t AUTOCG_SET
 
__IOM uint32_t AUTOCG_TGL
 
__IOM uint32_t AUXDATA
 
__IOM uint32_t AUXDATA_CLR
 
__IOM uint32_t AUXDATA_SET
 
__IOM uint32_t AUXDATA_TGL
 
__IOM uint32_t BLOCKRAMADDR
 
__IOM uint32_t BLOCKRAMADDR_CLR
 
__IOM uint32_t BLOCKRAMADDR_SET
 
__IOM uint32_t BLOCKRAMADDR_TGL
 
__IOM uint32_t BUFFERMODE
 
__IOM uint32_t BUFFERMODE_CLR
 
__IOM uint32_t BUFFERMODE_SET
 
__IOM uint32_t BUFFERMODE_TGL
 
__IOM uint32_t CGCLKSTOP
 
__IOM uint32_t CGCLKSTOP_CLR
 
__IOM uint32_t CGCLKSTOP_SET
 
__IOM uint32_t CGCLKSTOP_TGL
 
__IOM uint32_t CMD
 
__IOM uint32_t CMD_CLR
 
__IOM uint32_t CMD_SET
 
__IOM uint32_t CMD_TGL
 
__IOM uint32_t CONVGENERATOR
 
__IOM uint32_t CONVGENERATOR_CLR
 
__IOM uint32_t CONVGENERATOR_SET
 
__IOM uint32_t CONVGENERATOR_TGL
 
__IOM uint32_t CONVRAMADDR
 
__IOM uint32_t CONVRAMADDR_CLR
 
__IOM uint32_t CONVRAMADDR_SET
 
__IOM uint32_t CONVRAMADDR_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t DATABUFFER
 
__IOM uint32_t DATABUFFER_CLR
 
__IOM uint32_t DATABUFFER_SET
 
__IOM uint32_t DATABUFFER_TGL
 
__IOM uint32_t DFLCTRL
 
__IOM uint32_t DFLCTRL_CLR
 
__IOM uint32_t DFLCTRL_SET
 
__IOM uint32_t DFLCTRL_TGL
 
__IOM uint32_t EN
 
__IOM uint32_t EN_CLR
 
__IOM uint32_t EN_SET
 
__IOM uint32_t EN_TGL
 
FRC_FCD_TypeDef FCD [4U]
 
FRC_FCD_TypeDef FCD_CLR [4U]
 
FRC_FCD_TypeDef FCD_SET [4U]
 
FRC_FCD_TypeDef FCD_TGL [4U]
 
__IOM uint32_t FECCTRL
 
__IOM uint32_t FECCTRL_CLR
 
__IOM uint32_t FECCTRL_SET
 
__IOM uint32_t FECCTRL_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
FRC_INTELEMENT_TypeDef INTELEMENT [16U]
 
FRC_INTELEMENT_TypeDef INTELEMENT_CLR [16U]
 
FRC_INTELEMENT_TypeDef INTELEMENT_SET [16U]
 
FRC_INTELEMENT_TypeDef INTELEMENT_TGL [16U]
 
__IM uint32_t INTELEMENTNEXT
 
__IM uint32_t INTELEMENTNEXT_CLR
 
__IM uint32_t INTELEMENTNEXT_SET
 
__IM uint32_t INTELEMENTNEXT_TGL
 
__IOM uint32_t INTREADPOINT
 
__IOM uint32_t INTREADPOINT_CLR
 
__IOM uint32_t INTREADPOINT_SET
 
__IOM uint32_t INTREADPOINT_TGL
 
__IOM uint32_t INTWRITEPOINT
 
__IOM uint32_t INTWRITEPOINT_CLR
 
__IOM uint32_t INTWRITEPOINT_SET
 
__IOM uint32_t INTWRITEPOINT_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IM uint32_t LIKELYCONVSTATE
 
__IM uint32_t LIKELYCONVSTATE_CLR
 
__IM uint32_t LIKELYCONVSTATE_SET
 
__IM uint32_t LIKELYCONVSTATE_TGL
 
__IOM uint32_t MAXLENGTH
 
__IOM uint32_t MAXLENGTH_CLR
 
__IOM uint32_t MAXLENGTH_SET
 
__IOM uint32_t MAXLENGTH_TGL
 
__IOM uint32_t MIRRORIF
 
__IOM uint32_t MIRRORIF_CLR
 
__IOM uint32_t MIRRORIF_SET
 
__IOM uint32_t MIRRORIF_TGL
 
__IOM uint32_t PAUSECTRL
 
__IOM uint32_t PAUSECTRL_CLR
 
__IOM uint32_t PAUSECTRL_SET
 
__IOM uint32_t PAUSECTRL_TGL
 
__IM uint32_t PAUSEDATA
 
__IM uint32_t PAUSEDATA_CLR
 
__IM uint32_t PAUSEDATA_SET
 
__IM uint32_t PAUSEDATA_TGL
 
__IOM uint32_t PUNCTCTRL
 
__IOM uint32_t PUNCTCTRL_CLR
 
__IOM uint32_t PUNCTCTRL_SET
 
__IOM uint32_t PUNCTCTRL_TGL
 
__IOM uint32_t RAMBASEADDR
 
__IOM uint32_t RAMBASEADDR_CLR
 
__IOM uint32_t RAMBASEADDR_SET
 
__IOM uint32_t RAMBASEADDR_TGL
 
__IOM uint32_t RAWCTRL
 
__IOM uint32_t RAWCTRL_CLR
 
__IOM uint32_t RAWCTRL_SET
 
__IOM uint32_t RAWCTRL_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [2U]
 
uint32_t RESERVED10 [15U]
 
uint32_t RESERVED11 [944U]
 
uint32_t RESERVED12 [1U]
 
uint32_t RESERVED13 [2U]
 
uint32_t RESERVED14 [15U]
 
uint32_t RESERVED2 [15U]
 
uint32_t RESERVED3 [944U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [2U]
 
uint32_t RESERVED6 [15U]
 
uint32_t RESERVED7 [944U]
 
uint32_t RESERVED8 [1U]
 
uint32_t RESERVED9 [2U]
 
__IOM uint32_t RXCTRL
 
__IOM uint32_t RXCTRL_CLR
 
__IOM uint32_t RXCTRL_SET
 
__IOM uint32_t RXCTRL_TGL
 
__IM uint32_t RXRAWDATA
 
__IM uint32_t RXRAWDATA_CLR
 
__IM uint32_t RXRAWDATA_SET
 
__IM uint32_t RXRAWDATA_TGL
 
__IM uint32_t SCNT
 
__IM uint32_t SCNT_CLR
 
__IM uint32_t SCNT_SET
 
__IM uint32_t SCNT_TGL
 
__IOM uint32_t SNIFFCTRL
 
__IOM uint32_t SNIFFCTRL_CLR
 
__IOM uint32_t SNIFFCTRL_SET
 
__IOM uint32_t SNIFFCTRL_TGL
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 
__IOM uint32_t TRAILRXDATA
 
__IOM uint32_t TRAILRXDATA_CLR
 
__IOM uint32_t TRAILRXDATA_SET
 
__IOM uint32_t TRAILRXDATA_TGL
 
__IOM uint32_t TRAILTXDATACTRL
 
__IOM uint32_t TRAILTXDATACTRL_CLR
 
__IOM uint32_t TRAILTXDATACTRL_SET
 
__IOM uint32_t TRAILTXDATACTRL_TGL
 
__IM uint32_t WCNT
 
__IM uint32_t WCNT_CLR
 
__IM uint32_t WCNT_SET
 
__IM uint32_t WCNT_TGL
 
__IOM uint32_t WCNTCMP0
 
__IOM uint32_t WCNTCMP0_CLR
 
__IOM uint32_t WCNTCMP0_SET
 
__IOM uint32_t WCNTCMP0_TGL
 
__IOM uint32_t WCNTCMP1
 
__IOM uint32_t WCNTCMP1_CLR
 
__IOM uint32_t WCNTCMP1_SET
 
__IOM uint32_t WCNTCMP1_TGL
 
__IOM uint32_t WCNTCMP2
 
__IOM uint32_t WCNTCMP2_CLR
 
__IOM uint32_t WCNTCMP2_SET
 
__IOM uint32_t WCNTCMP2_TGL
 
__IOM uint32_t WHITECTRL
 
__IOM uint32_t WHITECTRL_CLR
 
__IOM uint32_t WHITECTRL_SET
 
__IOM uint32_t WHITECTRL_TGL
 
__IOM uint32_t WHITEINIT
 
__IOM uint32_t WHITEINIT_CLR
 
__IOM uint32_t WHITEINIT_SET
 
__IOM uint32_t WHITEINIT_TGL
 
__IOM uint32_t WHITEPOLY
 
__IOM uint32_t WHITEPOLY_CLR
 
__IOM uint32_t WHITEPOLY_SET
 
__IOM uint32_t WHITEPOLY_TGL
 

Field Documentation

__IOM uint32_t FRC_TypeDef::ADDRFILTCTRL

Address Filter Control

Definition at line 62 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::ADDRFILTCTRL_CLR

Address Filter Control

Definition at line 158 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::ADDRFILTCTRL_SET

Address Filter Control

Definition at line 110 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::ADDRFILTCTRL_TGL

Address Filter Control

Definition at line 206 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUTOCG

Automatic clock gating

Definition at line 98 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUTOCG_CLR

Automatic clock gating

Definition at line 194 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUTOCG_SET

Automatic clock gating

Definition at line 146 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUTOCG_TGL

Automatic clock gating

Definition at line 242 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUXDATA

Auxiliary sniffer data output register

Definition at line 90 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUXDATA_CLR

Auxiliary sniffer data output register

Definition at line 186 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUXDATA_SET

Auxiliary sniffer data output register

Definition at line 138 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::AUXDATA_TGL

Auxiliary sniffer data output register

Definition at line 234 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BLOCKRAMADDR

Block decoding RAM address register

Definition at line 73 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BLOCKRAMADDR_CLR

Block decoding RAM address register

Definition at line 169 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BLOCKRAMADDR_SET

Block decoding RAM address register

Definition at line 121 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BLOCKRAMADDR_TGL

Block decoding RAM address register

Definition at line 217 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BUFFERMODE

FRC Buffer Control

Definition at line 87 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BUFFERMODE_CLR

FRC Buffer Control

Definition at line 183 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BUFFERMODE_SET

FRC Buffer Control

Definition at line 135 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::BUFFERMODE_TGL

FRC Buffer Control

Definition at line 231 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CGCLKSTOP

Automatic clock gating

Definition at line 99 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CGCLKSTOP_CLR

Automatic clock gating

Definition at line 195 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CGCLKSTOP_SET

Automatic clock gating

Definition at line 147 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CGCLKSTOP_TGL

Automatic clock gating

Definition at line 243 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CMD

FRC Commands

Definition at line 68 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CMD_CLR

FRC Commands

Definition at line 164 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CMD_SET

FRC Commands

Definition at line 116 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CMD_TGL

FRC Commands

Definition at line 212 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVGENERATOR

Convolutional Coder Polynomials

Definition at line 80 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVGENERATOR_CLR

Convolutional Coder Polynomials

Definition at line 176 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVGENERATOR_SET

Convolutional Coder Polynomials

Definition at line 128 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVGENERATOR_TGL

Convolutional Coder Polynomials

Definition at line 224 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVRAMADDR

Convolutional decoding RAM address

Definition at line 74 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVRAMADDR_CLR

Convolutional decoding RAM address

Definition at line 170 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVRAMADDR_SET

Convolutional decoding RAM address

Definition at line 122 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CONVRAMADDR_TGL

Convolutional decoding RAM address

Definition at line 218 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CTRL

Control Register

Definition at line 75 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CTRL_CLR

Control Register

Definition at line 171 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CTRL_SET

Control Register

Definition at line 123 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::CTRL_TGL

Control Register

Definition at line 219 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DATABUFFER

Frame controller data buffer

Definition at line 63 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DATABUFFER_CLR

Frame controller data buffer

Definition at line 159 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DATABUFFER_SET

Frame controller data buffer

Definition at line 111 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DATABUFFER_TGL

Frame controller data buffer

Definition at line 207 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DFLCTRL

Dynamic Frame Length Control

Definition at line 60 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DFLCTRL_CLR

Dynamic Frame Length Control

Definition at line 156 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DFLCTRL_SET

Dynamic Frame Length Control

Definition at line 108 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::DFLCTRL_TGL

Dynamic Frame Length Control

Definition at line 204 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::EN

Enable peripheral clock to this module

Definition at line 58 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::EN_CLR

Enable peripheral clock to this module

Definition at line 154 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::EN_SET

Enable peripheral clock to this module

Definition at line 106 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::EN_TGL

Enable peripheral clock to this module

Definition at line 202 of file efr32bg21_frc.h.

FRC_FCD_TypeDef FRC_TypeDef::FCD[4U]

Frame Descriptors

Definition at line 101 of file efr32bg21_frc.h.

FRC_FCD_TypeDef FRC_TypeDef::FCD_CLR[4U]

Frame Descriptors

Definition at line 197 of file efr32bg21_frc.h.

FRC_FCD_TypeDef FRC_TypeDef::FCD_SET[4U]

Frame Descriptors

Definition at line 149 of file efr32bg21_frc.h.

FRC_FCD_TypeDef FRC_TypeDef::FCD_TGL[4U]

Frame Descriptors

Definition at line 245 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::FECCTRL

Forward Error Correction Control

Definition at line 72 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::FECCTRL_CLR

Forward Error Correction Control

Definition at line 168 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::FECCTRL_SET

Forward Error Correction Control

Definition at line 120 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::FECCTRL_TGL

Forward Error Correction Control

Definition at line 216 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IEN

Interrupt Enable Register

Definition at line 84 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 180 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 132 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 228 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IF

Frame Controller Interrupt Flags

Definition at line 83 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IF_CLR

Frame Controller Interrupt Flags

Definition at line 179 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IF_SET

Frame Controller Interrupt Flags

Definition at line 131 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::IF_TGL

Frame Controller Interrupt Flags

Definition at line 227 of file efr32bg21_frc.h.

FRC_INTELEMENT_TypeDef FRC_TypeDef::INTELEMENT[16U]

Interleaver element

Definition at line 103 of file efr32bg21_frc.h.

FRC_INTELEMENT_TypeDef FRC_TypeDef::INTELEMENT_CLR[16U]

Interleaver element

Definition at line 199 of file efr32bg21_frc.h.

FRC_INTELEMENT_TypeDef FRC_TypeDef::INTELEMENT_SET[16U]

Interleaver element

Definition at line 151 of file efr32bg21_frc.h.

FRC_INTELEMENT_TypeDef FRC_TypeDef::INTELEMENT_TGL[16U]

Interleaver element

Definition at line 247 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::INTELEMENTNEXT

Interleaver element value

Definition at line 95 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::INTELEMENTNEXT_CLR

Interleaver element value

Definition at line 191 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::INTELEMENTNEXT_SET

Interleaver element value

Definition at line 143 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::INTELEMENTNEXT_TGL

Interleaver element value

Definition at line 239 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTREADPOINT

Interleaver read pointer

Definition at line 97 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTREADPOINT_CLR

Interleaver read pointer

Definition at line 193 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTREADPOINT_SET

Interleaver read pointer

Definition at line 145 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTREADPOINT_TGL

Interleaver read pointer

Definition at line 241 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTWRITEPOINT

Interleaver write pointer

Definition at line 96 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTWRITEPOINT_CLR

Interleaver write pointer

Definition at line 192 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTWRITEPOINT_SET

Interleaver write pointer

Definition at line 144 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::INTWRITEPOINT_TGL

Interleaver write pointer

Definition at line 240 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::IPVERSION

IP Version

Definition at line 57 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::IPVERSION_CLR

IP Version

Definition at line 153 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::IPVERSION_SET

IP Version

Definition at line 105 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::IPVERSION_TGL

IP Version

Definition at line 201 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::LIKELYCONVSTATE

Most likely convolutional decoder state

Definition at line 94 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::LIKELYCONVSTATE_CLR

Most likely convolutional decoder state

Definition at line 190 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::LIKELYCONVSTATE_SET

Most likely convolutional decoder state

Definition at line 142 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::LIKELYCONVSTATE_TGL

Most likely convolutional decoder state

Definition at line 238 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MAXLENGTH

Maximum Frame Length Register

Definition at line 61 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MAXLENGTH_CLR

Maximum Frame Length Register

Definition at line 157 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MAXLENGTH_SET

Maximum Frame Length Register

Definition at line 109 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MAXLENGTH_TGL

Maximum Frame Length Register

Definition at line 205 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MIRRORIF

FRC Interrupt Flag Mirror Register

Definition at line 85 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MIRRORIF_CLR

FRC Interrupt Flag Mirror Register

Definition at line 181 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MIRRORIF_SET

FRC Interrupt Flag Mirror Register

Definition at line 133 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::MIRRORIF_TGL

FRC Interrupt Flag Mirror Register

Definition at line 229 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PAUSECTRL

Pause Control

Definition at line 82 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PAUSECTRL_CLR

Pause Control

Definition at line 178 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PAUSECTRL_SET

Pause Control

Definition at line 130 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PAUSECTRL_TGL

Pause Control

Definition at line 226 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::PAUSEDATA

Receiver pause data

Definition at line 93 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::PAUSEDATA_CLR

Receiver pause data

Definition at line 189 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::PAUSEDATA_SET

Receiver pause data

Definition at line 141 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::PAUSEDATA_TGL

Receiver pause data

Definition at line 237 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PUNCTCTRL

Puncturing Control

Definition at line 81 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PUNCTCTRL_CLR

Puncturing Control

Definition at line 177 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PUNCTCTRL_SET

Puncturing Control

Definition at line 129 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::PUNCTCTRL_TGL

Puncturing Control

Definition at line 225 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAMBASEADDR

RAM Base Address

Definition at line 100 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAMBASEADDR_CLR

RAM Base Address

Definition at line 196 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAMBASEADDR_SET

RAM Base Address

Definition at line 148 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAMBASEADDR_TGL

RAM Base Address

Definition at line 244 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAWCTRL

Raw data control

Definition at line 91 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAWCTRL_CLR

Raw data control

Definition at line 187 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAWCTRL_SET

Raw data control

Definition at line 139 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RAWCTRL_TGL

Raw data control

Definition at line 235 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 86 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED1[2U]

Reserved for future use

Definition at line 88 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED10[15U]

Reserved for future use

Definition at line 198 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED11[944U]

Reserved for future use

Definition at line 200 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED12[1U]

Reserved for future use

Definition at line 230 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED13[2U]

Reserved for future use

Definition at line 232 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED14[15U]

Reserved for future use

Definition at line 246 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED2[15U]

Reserved for future use

Definition at line 102 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED3[944U]

Reserved for future use

Definition at line 104 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 134 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED5[2U]

Reserved for future use

Definition at line 136 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED6[15U]

Reserved for future use

Definition at line 150 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED7[944U]

Reserved for future use

Definition at line 152 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED8[1U]

Reserved for future use

Definition at line 182 of file efr32bg21_frc.h.

uint32_t FRC_TypeDef::RESERVED9[2U]

Reserved for future use

Definition at line 184 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RXCTRL

RX Control Register

Definition at line 76 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RXCTRL_CLR

RX Control Register

Definition at line 172 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RXCTRL_SET

RX Control Register

Definition at line 124 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::RXCTRL_TGL

RX Control Register

Definition at line 220 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::RXRAWDATA

Receiver RAW data

Definition at line 92 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::RXRAWDATA_CLR

Receiver RAW data

Definition at line 188 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::RXRAWDATA_SET

Receiver RAW data

Definition at line 140 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::RXRAWDATA_TGL

Receiver RAW data

Definition at line 236 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::SCNT

Sub-Frame Counter Value Register

Definition at line 79 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::SCNT_CLR

Sub-Frame Counter Value Register

Definition at line 175 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::SCNT_SET

Sub-Frame Counter Value Register

Definition at line 127 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::SCNT_TGL

Sub-Frame Counter Value Register

Definition at line 223 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::SNIFFCTRL

FRC Sniffer Control Register

Definition at line 89 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::SNIFFCTRL_CLR

FRC Sniffer Control Register

Definition at line 185 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::SNIFFCTRL_SET

FRC Sniffer Control Register

Definition at line 137 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::SNIFFCTRL_TGL

FRC Sniffer Control Register

Definition at line 233 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::STATUS

FRC Status

Definition at line 59 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::STATUS_CLR

FRC Status

Definition at line 155 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::STATUS_SET

FRC Status

Definition at line 107 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::STATUS_TGL

FRC Status

Definition at line 203 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILRXDATA

Trailing RX Data

Definition at line 78 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILRXDATA_CLR

Trailing RX Data

Definition at line 174 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILRXDATA_SET

Trailing RX Data

Definition at line 126 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILRXDATA_TGL

Trailing RX Data

Definition at line 222 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILTXDATACTRL

Trailing TX Data Control

Definition at line 77 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILTXDATACTRL_CLR

Trailing TX Data Control

Definition at line 173 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILTXDATACTRL_SET

Trailing TX Data Control

Definition at line 125 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::TRAILTXDATACTRL_TGL

Trailing TX Data Control

Definition at line 221 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::WCNT

Word Counter Value Register

Definition at line 64 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::WCNT_CLR

Word Counter Value Register

Definition at line 160 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::WCNT_SET

Word Counter Value Register

Definition at line 112 of file efr32bg21_frc.h.

__IM uint32_t FRC_TypeDef::WCNT_TGL

Word Counter Value Register

Definition at line 208 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP0

Word Counter Compare 0

Definition at line 65 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP0_CLR

Word Counter Compare 0

Definition at line 161 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP0_SET

Word Counter Compare 0

Definition at line 113 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP0_TGL

Word Counter Compare 0

Definition at line 209 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP1

Word Counter Compare 1

Definition at line 66 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP1_CLR

Word Counter Compare 1

Definition at line 162 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP1_SET

Word Counter Compare 1

Definition at line 114 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP1_TGL

Word Counter Compare 1

Definition at line 210 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP2

Word Counter Compare 2

Definition at line 67 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP2_CLR

Word Counter Compare 2

Definition at line 163 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP2_SET

Word Counter Compare 2

Definition at line 115 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WCNTCMP2_TGL

Word Counter Compare 2

Definition at line 211 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITECTRL

Whitener Control

Definition at line 69 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITECTRL_CLR

Whitener Control

Definition at line 165 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITECTRL_SET

Whitener Control

Definition at line 117 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITECTRL_TGL

Whitener Control

Definition at line 213 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEINIT

Whitener Initial Value

Definition at line 71 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEINIT_CLR

Whitener Initial Value

Definition at line 167 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEINIT_SET

Whitener Initial Value

Definition at line 119 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEINIT_TGL

Whitener Initial Value

Definition at line 215 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEPOLY

Whitener Polynomial

Definition at line 70 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEPOLY_CLR

Whitener Polynomial

Definition at line 166 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEPOLY_SET

Whitener Polynomial

Definition at line 118 of file efr32bg21_frc.h.

__IOM uint32_t FRC_TypeDef::WHITEPOLY_TGL

Whitener Polynomial

Definition at line 214 of file efr32bg21_frc.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_frc.h