FSRCO_TypeDef Struct ReferenceDevices > FSRCO

FSRCO Register Declaration.

Definition at line 46 of file efr32bg21_fsrco.h.

#include <efr32bg21_fsrco.h>

Data Fields

__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
uint32_t RESERVED0 [1023U]
 
uint32_t RESERVED1 [1023U]
 
uint32_t RESERVED2 [1023U]
 

Field Documentation

__IM uint32_t FSRCO_TypeDef::IPVERSION

IP Version

Definition at line 47 of file efr32bg21_fsrco.h.

__IM uint32_t FSRCO_TypeDef::IPVERSION_CLR

IP Version

Definition at line 51 of file efr32bg21_fsrco.h.

__IM uint32_t FSRCO_TypeDef::IPVERSION_SET

IP Version

Definition at line 49 of file efr32bg21_fsrco.h.

__IM uint32_t FSRCO_TypeDef::IPVERSION_TGL

IP Version

Definition at line 53 of file efr32bg21_fsrco.h.

uint32_t FSRCO_TypeDef::RESERVED0[1023U]

Reserved for future use

Definition at line 48 of file efr32bg21_fsrco.h.

uint32_t FSRCO_TypeDef::RESERVED1[1023U]

Reserved for future use

Definition at line 50 of file efr32bg21_fsrco.h.

uint32_t FSRCO_TypeDef::RESERVED2[1023U]

Reserved for future use

Definition at line 52 of file efr32bg21_fsrco.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_fsrco.h