GPIO_ACMPROUTE_TypeDef Struct ReferenceDevices

Definition at line 42 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t ACMPOUTROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 

Field Documentation

__IOM uint32_t GPIO_ACMPROUTE_TypeDef::ACMPOUTROUTE

ACMPOUT port/pin select

Definition at line 44 of file efr32bg21_gpio.h.

uint32_t GPIO_ACMPROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 45 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_ACMPROUTE_TypeDef::ROUTEEN

ACMP0 pin enable

Definition at line 43 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h