GPIO_CMUROUTE_TypeDef Struct ReferenceDevices

Definition at line 48 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t CLKIN0ROUTE
 
__IOM uint32_t CLKOUT0ROUTE
 
__IOM uint32_t CLKOUT1ROUTE
 
__IOM uint32_t CLKOUT2ROUTE
 
uint32_t RESERVED0 [2U]
 
__IOM uint32_t ROUTEEN
 

Field Documentation

__IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKIN0ROUTE

CLKIN0 port/pin select

Definition at line 50 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKOUT0ROUTE

CLKOUT0 port/pin select

Definition at line 51 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKOUT1ROUTE

CLKOUT1 port/pin select

Definition at line 52 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKOUT2ROUTE

CLKOUT2 port/pin select

Definition at line 53 of file efr32bg21_gpio.h.

uint32_t GPIO_CMUROUTE_TypeDef::RESERVED0[2U]

Reserved for future use

Definition at line 54 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_CMUROUTE_TypeDef::ROUTEEN

CMU pin enable

Definition at line 49 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h