GPIO_FRCROUTE_TypeDef Struct ReferenceDevices

Definition at line 57 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t DCLKROUTE
 
__IOM uint32_t DFRAMEROUTE
 
__IOM uint32_t DOUTROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 

Field Documentation

__IOM uint32_t GPIO_FRCROUTE_TypeDef::DCLKROUTE

DCLK port/pin select

Definition at line 59 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_FRCROUTE_TypeDef::DFRAMEROUTE

DFRAME port/pin select

Definition at line 60 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_FRCROUTE_TypeDef::DOUTROUTE

DOUT port/pin select

Definition at line 61 of file efr32bg21_gpio.h.

uint32_t GPIO_FRCROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 62 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_FRCROUTE_TypeDef::ROUTEEN

FRC pin enable

Definition at line 58 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h