GPIO_LETIMERROUTE_TypeDef Struct ReferenceDevices

Definition at line 72 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t OUT0ROUTE
 
__IOM uint32_t OUT1ROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 

Field Documentation

__IOM uint32_t GPIO_LETIMERROUTE_TypeDef::OUT0ROUTE

OUT0 port/pin select

Definition at line 74 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_LETIMERROUTE_TypeDef::OUT1ROUTE

OUT1 port/pin select

Definition at line 75 of file efr32bg21_gpio.h.

uint32_t GPIO_LETIMERROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 76 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_LETIMERROUTE_TypeDef::ROUTEEN

LETIMER pin enable

Definition at line 73 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h