GPIO_MODEMROUTE_TypeDef Struct ReferenceDevices

Definition at line 79 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t ANT0ROUTE
 
__IOM uint32_t ANT1ROUTE
 
__IOM uint32_t DCLKROUTE
 
__IOM uint32_t DINROUTE
 
__IOM uint32_t DOUTROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 

Field Documentation

__IOM uint32_t GPIO_MODEMROUTE_TypeDef::ANT0ROUTE

ANT0 port/pin select

Definition at line 81 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_MODEMROUTE_TypeDef::ANT1ROUTE

ANT1 port/pin select

Definition at line 82 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_MODEMROUTE_TypeDef::DCLKROUTE

DCLK port/pin select

Definition at line 83 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_MODEMROUTE_TypeDef::DINROUTE

DIN port/pin select

Definition at line 84 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_MODEMROUTE_TypeDef::DOUTROUTE

DOUT port/pin select

Definition at line 85 of file efr32bg21_gpio.h.

uint32_t GPIO_MODEMROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 86 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_MODEMROUTE_TypeDef::ROUTEEN

MODEM pin enable

Definition at line 80 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h