GPIO_PORT_TypeDef Struct ReferenceDevices

EFR32BG21 GPIO PORT.

Definition at line 41 of file efr32bg21_gpio_port.h.

#include <efr32bg21_gpio_port.h>

Data Fields

__IOM uint32_t CTRL
 
__IM uint32_t DIN
 
__IOM uint32_t DOUT
 
__IOM uint32_t MODEH
 
__IOM uint32_t MODEL
 
uint32_t RESERVED0 [1]
 
uint32_t RESERVED1 [6]
 

Field Documentation

__IOM uint32_t GPIO_PORT_TypeDef::CTRL

Port control

Definition at line 42 of file efr32bg21_gpio_port.h.

__IM uint32_t GPIO_PORT_TypeDef::DIN

data in

Definition at line 47 of file efr32bg21_gpio_port.h.

__IOM uint32_t GPIO_PORT_TypeDef::DOUT

data out

Definition at line 46 of file efr32bg21_gpio_port.h.

__IOM uint32_t GPIO_PORT_TypeDef::MODEH

mode high

Definition at line 45 of file efr32bg21_gpio_port.h.

__IOM uint32_t GPIO_PORT_TypeDef::MODEL

mode low

Definition at line 43 of file efr32bg21_gpio_port.h.

uint32_t GPIO_PORT_TypeDef::RESERVED0[1]

Reserved for future use

Definition at line 44 of file efr32bg21_gpio_port.h.

uint32_t GPIO_PORT_TypeDef::RESERVED1[6]

Reserved for future use

Definition at line 48 of file efr32bg21_gpio_port.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio_port.h