GPIO_PRSROUTE_TypeDef Struct ReferenceDevices

Definition at line 89 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t ASYNCH0ROUTE
 
__IOM uint32_t ASYNCH10ROUTE
 
__IOM uint32_t ASYNCH11ROUTE
 
__IOM uint32_t ASYNCH1ROUTE
 
__IOM uint32_t ASYNCH2ROUTE
 
__IOM uint32_t ASYNCH3ROUTE
 
__IOM uint32_t ASYNCH4ROUTE
 
__IOM uint32_t ASYNCH5ROUTE
 
__IOM uint32_t ASYNCH6ROUTE
 
__IOM uint32_t ASYNCH7ROUTE
 
__IOM uint32_t ASYNCH8ROUTE
 
__IOM uint32_t ASYNCH9ROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 
__IOM uint32_t SYNCH0ROUTE
 
__IOM uint32_t SYNCH1ROUTE
 
__IOM uint32_t SYNCH2ROUTE
 
__IOM uint32_t SYNCH3ROUTE
 

Field Documentation

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH0ROUTE

ASYNCH0 port/pin select

Definition at line 91 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH10ROUTE

ASYNCH10 port/pin select

Definition at line 101 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH11ROUTE

ASYNCH11 port/pin select

Definition at line 102 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH1ROUTE

ASYNCH1 port/pin select

Definition at line 92 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH2ROUTE

ASYNCH2 port/pin select

Definition at line 93 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH3ROUTE

ASYNCH3 port/pin select

Definition at line 94 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH4ROUTE

ASYNCH4 port/pin select

Definition at line 95 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH5ROUTE

ASYNCH5 port/pin select

Definition at line 96 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH6ROUTE

ASYNCH6 port/pin select

Definition at line 97 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH7ROUTE

ASYNCH7 port/pin select

Definition at line 98 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH8ROUTE

ASYNCH8 port/pin select

Definition at line 99 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ASYNCH9ROUTE

ASYNCH9 port/pin select

Definition at line 100 of file efr32bg21_gpio.h.

uint32_t GPIO_PRSROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 107 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::ROUTEEN

PRS0 pin enable

Definition at line 90 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH0ROUTE

SYNCH0 port/pin select

Definition at line 103 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH1ROUTE

SYNCH1 port/pin select

Definition at line 104 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH2ROUTE

SYNCH2 port/pin select

Definition at line 105 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_PRSROUTE_TypeDef::SYNCH3ROUTE

SYNCH3 port/pin select

Definition at line 106 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h