GPIO_TIMERROUTE_TypeDef Struct ReferenceDevices

Definition at line 110 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t CC0ROUTE
 
__IOM uint32_t CC1ROUTE
 
__IOM uint32_t CC2ROUTE
 
__IOM uint32_t CDTI0ROUTE
 
__IOM uint32_t CDTI1ROUTE
 
__IOM uint32_t CDTI2ROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 

Field Documentation

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::CC0ROUTE

CC0 port/pin select

Definition at line 112 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::CC1ROUTE

CC1 port/pin select

Definition at line 113 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::CC2ROUTE

CC2 port/pin select

Definition at line 114 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::CDTI0ROUTE

CDTI0 port/pin select

Definition at line 115 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::CDTI1ROUTE

CDTI1 port/pin select

Definition at line 116 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::CDTI2ROUTE

CDTI2 port/pin select

Definition at line 117 of file efr32bg21_gpio.h.

uint32_t GPIO_TIMERROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 118 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TIMERROUTE_TypeDef::ROUTEEN

TIMER0 pin enable

Definition at line 111 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h