GPIO_TypeDef Struct ReferenceDevices

Definition at line 132 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t ABUSALLOC
 
__IOM uint32_t ABUSALLOC_CLR
 
__IOM uint32_t ABUSALLOC_SET
 
__IOM uint32_t ABUSALLOC_TGL
 
GPIO_ACMPROUTE_TypeDef ACMPROUTE [2U]
 
GPIO_ACMPROUTE_TypeDef ACMPROUTE_CLR [2U]
 
GPIO_ACMPROUTE_TypeDef ACMPROUTE_SET [2U]
 
GPIO_ACMPROUTE_TypeDef ACMPROUTE_TGL [2U]
 
__IOM uint32_t BBUSALLOC
 
__IOM uint32_t BBUSALLOC_CLR
 
__IOM uint32_t BBUSALLOC_SET
 
__IOM uint32_t BBUSALLOC_TGL
 
__IOM uint32_t CDBUSALLOC
 
__IOM uint32_t CDBUSALLOC_CLR
 
__IOM uint32_t CDBUSALLOC_SET
 
__IOM uint32_t CDBUSALLOC_TGL
 
GPIO_CMUROUTE_TypeDef CMUROUTE
 
GPIO_CMUROUTE_TypeDef CMUROUTE_CLR
 
GPIO_CMUROUTE_TypeDef CMUROUTE_SET
 
GPIO_CMUROUTE_TypeDef CMUROUTE_TGL
 
__IOM uint32_t DBGROUTEPEN
 
__IOM uint32_t DBGROUTEPEN_CLR
 
__IOM uint32_t DBGROUTEPEN_SET
 
__IOM uint32_t DBGROUTEPEN_TGL
 
__IOM uint32_t EM4WUEN
 
__IOM uint32_t EM4WUEN_CLR
 
__IOM uint32_t EM4WUEN_SET
 
__IOM uint32_t EM4WUEN_TGL
 
__IOM uint32_t EM4WUPOL
 
__IOM uint32_t EM4WUPOL_CLR
 
__IOM uint32_t EM4WUPOL_SET
 
__IOM uint32_t EM4WUPOL_TGL
 
__IOM uint32_t EXTIFALL
 
__IOM uint32_t EXTIFALL_CLR
 
__IOM uint32_t EXTIFALL_SET
 
__IOM uint32_t EXTIFALL_TGL
 
__IOM uint32_t EXTIPINSELL
 
__IOM uint32_t EXTIPINSELL_CLR
 
__IOM uint32_t EXTIPINSELL_SET
 
__IOM uint32_t EXTIPINSELL_TGL
 
__IOM uint32_t EXTIPSELL
 
__IOM uint32_t EXTIPSELL_CLR
 
__IOM uint32_t EXTIPSELL_SET
 
__IOM uint32_t EXTIPSELL_TGL
 
__IOM uint32_t EXTIRISE
 
__IOM uint32_t EXTIRISE_CLR
 
__IOM uint32_t EXTIRISE_SET
 
__IOM uint32_t EXTIRISE_TGL
 
GPIO_FRCROUTE_TypeDef FRCROUTE
 
GPIO_FRCROUTE_TypeDef FRCROUTE_CLR
 
GPIO_FRCROUTE_TypeDef FRCROUTE_SET
 
GPIO_FRCROUTE_TypeDef FRCROUTE_TGL
 
__IM uint32_t GPIOLOCKSTATUS
 
__IM uint32_t GPIOLOCKSTATUS_CLR
 
__IM uint32_t GPIOLOCKSTATUS_SET
 
__IM uint32_t GPIOLOCKSTATUS_TGL
 
GPIO_I2CROUTE_TypeDef I2CROUTE [2U]
 
GPIO_I2CROUTE_TypeDef I2CROUTE_CLR [2U]
 
GPIO_I2CROUTE_TypeDef I2CROUTE_SET [2U]
 
GPIO_I2CROUTE_TypeDef I2CROUTE_TGL [2U]
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
GPIO_LETIMERROUTE_TypeDef LETIMERROUTE [1U]
 
GPIO_LETIMERROUTE_TypeDef LETIMERROUTE_CLR [1U]
 
GPIO_LETIMERROUTE_TypeDef LETIMERROUTE_SET [1U]
 
GPIO_LETIMERROUTE_TypeDef LETIMERROUTE_TGL [1U]
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
GPIO_MODEMROUTE_TypeDef MODEMROUTE
 
GPIO_MODEMROUTE_TypeDef MODEMROUTE_CLR
 
GPIO_MODEMROUTE_TypeDef MODEMROUTE_SET
 
GPIO_MODEMROUTE_TypeDef MODEMROUTE_TGL
 
GPIO_PORT_TypeDef P [4U]
 
GPIO_PORT_TypeDef P_CLR [4U]
 
GPIO_PORT_TypeDef P_SET [4U]
 
GPIO_PORT_TypeDef P_TGL [4U]
 
GPIO_PRSROUTE_TypeDef PRSROUTE [1U]
 
GPIO_PRSROUTE_TypeDef PRSROUTE_CLR [1U]
 
GPIO_PRSROUTE_TypeDef PRSROUTE_SET [1U]
 
GPIO_PRSROUTE_TypeDef PRSROUTE_TGL [1U]
 
uint32_t RESERVED0 [144U]
 
uint32_t RESERVED1 [3U]
 
uint32_t RESERVED10 [637U]
 
uint32_t RESERVED11 [144U]
 
uint32_t RESERVED12 [3U]
 
uint32_t RESERVED13 [3U]
 
uint32_t RESERVED14 [53U]
 
uint32_t RESERVED15 [1U]
 
uint32_t RESERVED16 [1U]
 
uint32_t RESERVED17 [2U]
 
uint32_t RESERVED18 [1U]
 
uint32_t RESERVED19 [3U]
 
uint32_t RESERVED2 [3U]
 
uint32_t RESERVED20 [2U]
 
uint32_t RESERVED21 [637U]
 
uint32_t RESERVED22 [144U]
 
uint32_t RESERVED23 [3U]
 
uint32_t RESERVED24 [3U]
 
uint32_t RESERVED25 [53U]
 
uint32_t RESERVED26 [1U]
 
uint32_t RESERVED27 [1U]
 
uint32_t RESERVED28 [2U]
 
uint32_t RESERVED29 [1U]
 
uint32_t RESERVED3 [53U]
 
uint32_t RESERVED30 [3U]
 
uint32_t RESERVED31 [2U]
 
uint32_t RESERVED32 [637U]
 
uint32_t RESERVED33 [144U]
 
uint32_t RESERVED34 [3U]
 
uint32_t RESERVED35 [3U]
 
uint32_t RESERVED36 [53U]
 
uint32_t RESERVED37 [1U]
 
uint32_t RESERVED38 [1U]
 
uint32_t RESERVED39 [2U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED40 [1U]
 
uint32_t RESERVED41 [3U]
 
uint32_t RESERVED42 [2U]
 
uint32_t RESERVED5 [1U]
 
uint32_t RESERVED6 [2U]
 
uint32_t RESERVED7 [1U]
 
uint32_t RESERVED8 [3U]
 
uint32_t RESERVED9 [2U]
 
GPIO_TIMERROUTE_TypeDef TIMERROUTE [4U]
 
GPIO_TIMERROUTE_TypeDef TIMERROUTE_CLR [4U]
 
GPIO_TIMERROUTE_TypeDef TIMERROUTE_SET [4U]
 
GPIO_TIMERROUTE_TypeDef TIMERROUTE_TGL [4U]
 
__IOM uint32_t TRACEROUTEPEN
 
__IOM uint32_t TRACEROUTEPEN_CLR
 
__IOM uint32_t TRACEROUTEPEN_SET
 
__IOM uint32_t TRACEROUTEPEN_TGL
 
GPIO_USARTROUTE_TypeDef USARTROUTE [3U]
 
GPIO_USARTROUTE_TypeDef USARTROUTE_CLR [3U]
 
GPIO_USARTROUTE_TypeDef USARTROUTE_SET [3U]
 
GPIO_USARTROUTE_TypeDef USARTROUTE_TGL [3U]
 

Field Documentation

__IOM uint32_t GPIO_TypeDef::ABUSALLOC

A Bus allocation

Definition at line 139 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::ABUSALLOC_CLR

A Bus allocation

Definition at line 211 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::ABUSALLOC_SET

A Bus allocation

Definition at line 175 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::ABUSALLOC_TGL

A Bus allocation

Definition at line 247 of file efr32bg21_gpio.h.

GPIO_ACMPROUTE_TypeDef GPIO_TypeDef::ACMPROUTE[2U]

acmp0 DBUS config registers

Definition at line 159 of file efr32bg21_gpio.h.

GPIO_ACMPROUTE_TypeDef GPIO_TypeDef::ACMPROUTE_CLR[2U]

acmp0 DBUS config registers

Definition at line 231 of file efr32bg21_gpio.h.

GPIO_ACMPROUTE_TypeDef GPIO_TypeDef::ACMPROUTE_SET[2U]

acmp0 DBUS config registers

Definition at line 195 of file efr32bg21_gpio.h.

GPIO_ACMPROUTE_TypeDef GPIO_TypeDef::ACMPROUTE_TGL[2U]

acmp0 DBUS config registers

Definition at line 267 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::BBUSALLOC

B Bus allocation

Definition at line 140 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::BBUSALLOC_CLR

B Bus allocation

Definition at line 212 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::BBUSALLOC_SET

B Bus allocation

Definition at line 176 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::BBUSALLOC_TGL

B Bus allocation

Definition at line 248 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::CDBUSALLOC

CD Bus allocation

Definition at line 141 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::CDBUSALLOC_CLR

CD Bus allocation

Definition at line 213 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::CDBUSALLOC_SET

CD Bus allocation

Definition at line 177 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::CDBUSALLOC_TGL

CD Bus allocation

Definition at line 249 of file efr32bg21_gpio.h.

GPIO_CMUROUTE_TypeDef GPIO_TypeDef::CMUROUTE

cmu DBUS config registers

Definition at line 160 of file efr32bg21_gpio.h.

GPIO_CMUROUTE_TypeDef GPIO_TypeDef::CMUROUTE_CLR

cmu DBUS config registers

Definition at line 232 of file efr32bg21_gpio.h.

GPIO_CMUROUTE_TypeDef GPIO_TypeDef::CMUROUTE_SET

cmu DBUS config registers

Definition at line 196 of file efr32bg21_gpio.h.

GPIO_CMUROUTE_TypeDef GPIO_TypeDef::CMUROUTE_TGL

cmu DBUS config registers

Definition at line 268 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::DBGROUTEPEN

Debugger Route Pin enable

Definition at line 156 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::DBGROUTEPEN_CLR

Debugger Route Pin enable

Definition at line 228 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::DBGROUTEPEN_SET

Debugger Route Pin enable

Definition at line 192 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::DBGROUTEPEN_TGL

Debugger Route Pin enable

Definition at line 264 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUEN

main

Definition at line 153 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUEN_CLR

main

Definition at line 225 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUEN_SET

main

Definition at line 189 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUEN_TGL

main

Definition at line 261 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUPOL

New Register

Definition at line 154 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUPOL_CLR

New Register

Definition at line 226 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUPOL_SET

New Register

Definition at line 190 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EM4WUPOL_TGL

New Register

Definition at line 262 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIFALL

External Interrupt Falling Edge Trigger

Definition at line 148 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIFALL_CLR

External Interrupt Falling Edge Trigger

Definition at line 220 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIFALL_SET

External Interrupt Falling Edge Trigger

Definition at line 184 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIFALL_TGL

External Interrupt Falling Edge Trigger

Definition at line 256 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPINSELL

External Interrupt Pin Select Low

Definition at line 145 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPINSELL_CLR

External Interrupt Pin Select Low

Definition at line 217 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPINSELL_SET

External Interrupt Pin Select Low

Definition at line 181 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPINSELL_TGL

External Interrupt Pin Select Low

Definition at line 253 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPSELL

External Interrupt Port Select Low

Definition at line 143 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPSELL_CLR

External Interrupt Port Select Low

Definition at line 215 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPSELL_SET

External Interrupt Port Select Low

Definition at line 179 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIPSELL_TGL

External Interrupt Port Select Low

Definition at line 251 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIRISE

External Interrupt Rising Edge Trigger

Definition at line 147 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIRISE_CLR

External Interrupt Rising Edge Trigger

Definition at line 219 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIRISE_SET

External Interrupt Rising Edge Trigger

Definition at line 183 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::EXTIRISE_TGL

External Interrupt Rising Edge Trigger

Definition at line 255 of file efr32bg21_gpio.h.

GPIO_FRCROUTE_TypeDef GPIO_TypeDef::FRCROUTE

frc DBUS config registers

Definition at line 161 of file efr32bg21_gpio.h.

GPIO_FRCROUTE_TypeDef GPIO_TypeDef::FRCROUTE_CLR

frc DBUS config registers

Definition at line 233 of file efr32bg21_gpio.h.

GPIO_FRCROUTE_TypeDef GPIO_TypeDef::FRCROUTE_SET

frc DBUS config registers

Definition at line 197 of file efr32bg21_gpio.h.

GPIO_FRCROUTE_TypeDef GPIO_TypeDef::FRCROUTE_TGL

frc DBUS config registers

Definition at line 269 of file efr32bg21_gpio.h.

__IM uint32_t GPIO_TypeDef::GPIOLOCKSTATUS

Lock Status

Definition at line 137 of file efr32bg21_gpio.h.

__IM uint32_t GPIO_TypeDef::GPIOLOCKSTATUS_CLR

Lock Status

Definition at line 209 of file efr32bg21_gpio.h.

__IM uint32_t GPIO_TypeDef::GPIOLOCKSTATUS_SET

Lock Status

Definition at line 173 of file efr32bg21_gpio.h.

__IM uint32_t GPIO_TypeDef::GPIOLOCKSTATUS_TGL

Lock Status

Definition at line 245 of file efr32bg21_gpio.h.

GPIO_I2CROUTE_TypeDef GPIO_TypeDef::I2CROUTE[2U]

i2c0 DBUS config registers

Definition at line 162 of file efr32bg21_gpio.h.

GPIO_I2CROUTE_TypeDef GPIO_TypeDef::I2CROUTE_CLR[2U]

i2c0 DBUS config registers

Definition at line 234 of file efr32bg21_gpio.h.

GPIO_I2CROUTE_TypeDef GPIO_TypeDef::I2CROUTE_SET[2U]

i2c0 DBUS config registers

Definition at line 198 of file efr32bg21_gpio.h.

GPIO_I2CROUTE_TypeDef GPIO_TypeDef::I2CROUTE_TGL[2U]

i2c0 DBUS config registers

Definition at line 270 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IEN

Interrupt Enable

Definition at line 151 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IEN_CLR

Interrupt Enable

Definition at line 223 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IEN_SET

Interrupt Enable

Definition at line 187 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IEN_TGL

Interrupt Enable

Definition at line 259 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IF

Interrupt Flag

Definition at line 150 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IF_CLR

Interrupt Flag

Definition at line 222 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IF_SET

Interrupt Flag

Definition at line 186 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::IF_TGL

Interrupt Flag

Definition at line 258 of file efr32bg21_gpio.h.

GPIO_LETIMERROUTE_TypeDef GPIO_TypeDef::LETIMERROUTE[1U]

letimer DBUS config registers

Definition at line 163 of file efr32bg21_gpio.h.

GPIO_LETIMERROUTE_TypeDef GPIO_TypeDef::LETIMERROUTE_CLR[1U]

letimer DBUS config registers

Definition at line 235 of file efr32bg21_gpio.h.

GPIO_LETIMERROUTE_TypeDef GPIO_TypeDef::LETIMERROUTE_SET[1U]

letimer DBUS config registers

Definition at line 199 of file efr32bg21_gpio.h.

GPIO_LETIMERROUTE_TypeDef GPIO_TypeDef::LETIMERROUTE_TGL[1U]

letimer DBUS config registers

Definition at line 271 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::LOCK

main

Definition at line 135 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::LOCK_CLR

main

Definition at line 207 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::LOCK_SET

main

Definition at line 171 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::LOCK_TGL

main

Definition at line 243 of file efr32bg21_gpio.h.

GPIO_MODEMROUTE_TypeDef GPIO_TypeDef::MODEMROUTE

modem DBUS config registers

Definition at line 164 of file efr32bg21_gpio.h.

GPIO_MODEMROUTE_TypeDef GPIO_TypeDef::MODEMROUTE_CLR

modem DBUS config registers

Definition at line 236 of file efr32bg21_gpio.h.

GPIO_MODEMROUTE_TypeDef GPIO_TypeDef::MODEMROUTE_SET

modem DBUS config registers

Definition at line 200 of file efr32bg21_gpio.h.

GPIO_MODEMROUTE_TypeDef GPIO_TypeDef::MODEMROUTE_TGL

modem DBUS config registers

Definition at line 272 of file efr32bg21_gpio.h.

GPIO_PRSROUTE_TypeDef GPIO_TypeDef::PRSROUTE[1U]

prs0 DBUS config registers

Definition at line 165 of file efr32bg21_gpio.h.

GPIO_PRSROUTE_TypeDef GPIO_TypeDef::PRSROUTE_CLR[1U]

prs0 DBUS config registers

Definition at line 237 of file efr32bg21_gpio.h.

GPIO_PRSROUTE_TypeDef GPIO_TypeDef::PRSROUTE_SET[1U]

prs0 DBUS config registers

Definition at line 201 of file efr32bg21_gpio.h.

GPIO_PRSROUTE_TypeDef GPIO_TypeDef::PRSROUTE_TGL[1U]

prs0 DBUS config registers

Definition at line 273 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED0[144U]

Reserved for future use

Definition at line 134 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED1[3U]

Reserved for future use

Definition at line 136 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED10[637U]

Reserved for future use

Definition at line 168 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED11[144U]

Reserved for future use

Definition at line 170 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED12[3U]

Reserved for future use

Definition at line 172 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED13[3U]

Reserved for future use

Definition at line 174 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED14[53U]

Reserved for future use

Definition at line 178 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED15[1U]

Reserved for future use

Definition at line 180 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED16[1U]

Reserved for future use

Definition at line 182 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED17[2U]

Reserved for future use

Definition at line 185 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED18[1U]

Reserved for future use

Definition at line 188 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED19[3U]

Reserved for future use

Definition at line 191 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED2[3U]

Reserved for future use

Definition at line 138 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED20[2U]

Reserved for future use

Definition at line 194 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED21[637U]

Reserved for future use

Definition at line 204 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED22[144U]

Reserved for future use

Definition at line 206 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED23[3U]

Reserved for future use

Definition at line 208 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED24[3U]

Reserved for future use

Definition at line 210 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED25[53U]

Reserved for future use

Definition at line 214 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED26[1U]

Reserved for future use

Definition at line 216 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED27[1U]

Reserved for future use

Definition at line 218 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED28[2U]

Reserved for future use

Definition at line 221 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED29[1U]

Reserved for future use

Definition at line 224 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED3[53U]

Reserved for future use

Definition at line 142 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED30[3U]

Reserved for future use

Definition at line 227 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED31[2U]

Reserved for future use

Definition at line 230 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED32[637U]

Reserved for future use

Definition at line 240 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED33[144U]

Reserved for future use

Definition at line 242 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED34[3U]

Reserved for future use

Definition at line 244 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED35[3U]

Reserved for future use

Definition at line 246 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED36[53U]

Reserved for future use

Definition at line 250 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED37[1U]

Reserved for future use

Definition at line 252 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED38[1U]

Reserved for future use

Definition at line 254 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED39[2U]

Reserved for future use

Definition at line 257 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 144 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED40[1U]

Reserved for future use

Definition at line 260 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED41[3U]

Reserved for future use

Definition at line 263 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED42[2U]

Reserved for future use

Definition at line 266 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED5[1U]

Reserved for future use

Definition at line 146 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED6[2U]

Reserved for future use

Definition at line 149 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED7[1U]

Reserved for future use

Definition at line 152 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED8[3U]

Reserved for future use

Definition at line 155 of file efr32bg21_gpio.h.

uint32_t GPIO_TypeDef::RESERVED9[2U]

Reserved for future use

Definition at line 158 of file efr32bg21_gpio.h.

GPIO_TIMERROUTE_TypeDef GPIO_TypeDef::TIMERROUTE[4U]

timer0 DBUS config registers

Definition at line 166 of file efr32bg21_gpio.h.

GPIO_TIMERROUTE_TypeDef GPIO_TypeDef::TIMERROUTE_CLR[4U]

timer0 DBUS config registers

Definition at line 238 of file efr32bg21_gpio.h.

GPIO_TIMERROUTE_TypeDef GPIO_TypeDef::TIMERROUTE_SET[4U]

timer0 DBUS config registers

Definition at line 202 of file efr32bg21_gpio.h.

GPIO_TIMERROUTE_TypeDef GPIO_TypeDef::TIMERROUTE_TGL[4U]

timer0 DBUS config registers

Definition at line 274 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::TRACEROUTEPEN

Trace Route Pin Enable

Definition at line 157 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::TRACEROUTEPEN_CLR

Trace Route Pin Enable

Definition at line 229 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::TRACEROUTEPEN_SET

Trace Route Pin Enable

Definition at line 193 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_TypeDef::TRACEROUTEPEN_TGL

Trace Route Pin Enable

Definition at line 265 of file efr32bg21_gpio.h.

GPIO_USARTROUTE_TypeDef GPIO_TypeDef::USARTROUTE[3U]

usart0 DBUS config registers

Definition at line 167 of file efr32bg21_gpio.h.

GPIO_USARTROUTE_TypeDef GPIO_TypeDef::USARTROUTE_CLR[3U]

usart0 DBUS config registers

Definition at line 239 of file efr32bg21_gpio.h.

GPIO_USARTROUTE_TypeDef GPIO_TypeDef::USARTROUTE_SET[3U]

usart0 DBUS config registers

Definition at line 203 of file efr32bg21_gpio.h.

GPIO_USARTROUTE_TypeDef GPIO_TypeDef::USARTROUTE_TGL[3U]

usart0 DBUS config registers

Definition at line 275 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h