GPIO_USARTROUTE_TypeDef Struct ReferenceDevices

Definition at line 121 of file efr32bg21_gpio.h.

Data Fields

__IOM uint32_t CLKROUTE
 
__IOM uint32_t CSROUTE
 
__IOM uint32_t CTSROUTE
 
uint32_t RESERVED0 [1U]
 
__IOM uint32_t ROUTEEN
 
__IOM uint32_t RTSROUTE
 
__IOM uint32_t RXROUTE
 
__IOM uint32_t TXROUTE
 

Field Documentation

__IOM uint32_t GPIO_USARTROUTE_TypeDef::CLKROUTE

CLK port/pin select

Definition at line 127 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_USARTROUTE_TypeDef::CSROUTE

CS port/pin select

Definition at line 123 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_USARTROUTE_TypeDef::CTSROUTE

CTS port/pin select

Definition at line 124 of file efr32bg21_gpio.h.

uint32_t GPIO_USARTROUTE_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 129 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_USARTROUTE_TypeDef::ROUTEEN

USART0 pin enable

Definition at line 122 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_USARTROUTE_TypeDef::RTSROUTE

RTS port/pin select

Definition at line 125 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_USARTROUTE_TypeDef::RXROUTE

RX port/pin select

Definition at line 126 of file efr32bg21_gpio.h.

__IOM uint32_t GPIO_USARTROUTE_TypeDef::TXROUTE

TX port/pin select

Definition at line 128 of file efr32bg21_gpio.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_gpio.h