HFRCO_TypeDef Struct ReferenceDevices > HFRCO

HFRCO Register Declaration.

Definition at line 46 of file efr32bg21_hfrco.h.

#include <efr32bg21_hfrco.h>

Data Fields

__IOM uint32_t CAL
 
__IOM uint32_t CAL_CLR
 
__IOM uint32_t CAL_SET
 
__IOM uint32_t CAL_TGL
 
__IOM uint32_t CTRL
 
__IOM uint32_t CTRL_CLR
 
__IOM uint32_t CTRL_SET
 
__IOM uint32_t CTRL_TGL
 
__IOM uint32_t IEN
 
__IOM uint32_t IEN_CLR
 
__IOM uint32_t IEN_SET
 
__IOM uint32_t IEN_TGL
 
__IOM uint32_t IF
 
__IOM uint32_t IF_CLR
 
__IOM uint32_t IF_SET
 
__IOM uint32_t IF_TGL
 
__IM uint32_t IPVERSION
 
__IM uint32_t IPVERSION_CLR
 
__IM uint32_t IPVERSION_SET
 
__IM uint32_t IPVERSION_TGL
 
__IOM uint32_t LOCK
 
__IOM uint32_t LOCK_CLR
 
__IOM uint32_t LOCK_SET
 
__IOM uint32_t LOCK_TGL
 
uint32_t RESERVED0 [1U]
 
uint32_t RESERVED1 [1016U]
 
uint32_t RESERVED2 [1U]
 
uint32_t RESERVED3 [1016U]
 
uint32_t RESERVED4 [1U]
 
uint32_t RESERVED5 [1016U]
 
uint32_t RESERVED6 [1U]
 
__IM uint32_t STATUS
 
__IM uint32_t STATUS_CLR
 
__IM uint32_t STATUS_SET
 
__IM uint32_t STATUS_TGL
 

Field Documentation

__IOM uint32_t HFRCO_TypeDef::CAL

Calibration Register

Definition at line 49 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CAL_CLR

Calibration Register

Definition at line 67 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CAL_SET

Calibration Register

Definition at line 58 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CAL_TGL

Calibration Register

Definition at line 76 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CTRL

Ctrl Register

Definition at line 48 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CTRL_CLR

Ctrl Register

Definition at line 66 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CTRL_SET

Ctrl Register

Definition at line 57 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::CTRL_TGL

Ctrl Register

Definition at line 75 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IEN

Interrupt Enable Register

Definition at line 52 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IEN_CLR

Interrupt Enable Register

Definition at line 70 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IEN_SET

Interrupt Enable Register

Definition at line 61 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IEN_TGL

Interrupt Enable Register

Definition at line 79 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IF

Interrupt Flag Register

Definition at line 51 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IF_CLR

Interrupt Flag Register

Definition at line 69 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IF_SET

Interrupt Flag Register

Definition at line 60 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::IF_TGL

Interrupt Flag Register

Definition at line 78 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::IPVERSION

IP Version ID

Definition at line 47 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::IPVERSION_CLR

IP Version ID

Definition at line 65 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::IPVERSION_SET

IP Version ID

Definition at line 56 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::IPVERSION_TGL

IP Version ID

Definition at line 74 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::LOCK

Lock Register

Definition at line 54 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::LOCK_CLR

Lock Register

Definition at line 72 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::LOCK_SET

Lock Register

Definition at line 63 of file efr32bg21_hfrco.h.

__IOM uint32_t HFRCO_TypeDef::LOCK_TGL

Lock Register

Definition at line 81 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED0[1U]

Reserved for future use

Definition at line 53 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED1[1016U]

Reserved for future use

Definition at line 55 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED2[1U]

Reserved for future use

Definition at line 62 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED3[1016U]

Reserved for future use

Definition at line 64 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED4[1U]

Reserved for future use

Definition at line 71 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED5[1016U]

Reserved for future use

Definition at line 73 of file efr32bg21_hfrco.h.

uint32_t HFRCO_TypeDef::RESERVED6[1U]

Reserved for future use

Definition at line 80 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::STATUS

Status Register

Definition at line 50 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::STATUS_CLR

Status Register

Definition at line 68 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::STATUS_SET

Status Register

Definition at line 59 of file efr32bg21_hfrco.h.

__IM uint32_t HFRCO_TypeDef::STATUS_TGL

Status Register

Definition at line 77 of file efr32bg21_hfrco.h.


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/efr32bg21_hfrco.h